Customer Reviews of Screw Type 415EA, Swivel Caster With Stopper, Rubber Solid Wheel,
|
Sales Price: 5.99 SGD
Review Rating:
![]() 11 Customer Reviews
|
|
---|
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
As a caster for industrial sewing machines

From Japan
On 2018-03-18 08:01:22
There is no problem because it is a hammer, but since the sewing machine has about 40 to 50 kg
If it does not move for a long time, the rubber wheel deforms «The load resistance is cleared» but the rubber wheel is deformed, the plastic wheel can not be fixed, either can not be satisfied
This review is about item#02212314.
Work parts for industrial high school work.

From Japan
On 2018-01-29 17:57:51
I purchased it because it is compatible with small lot and kind.
This review is about item#2212323.
Movement of cutting machine

From Japan
On 2017-09-15 16:10:02
Although it was white with a hard wheel from the beginning, since vibration and sound were great when moving, it became possible to exchange quietly with rubber.
This review is about item#02212271.
For signs

From Japan
On 2017-07-15 16:43:54
When asking a merchant, a place to be expensive - the trader taught me that I'm buying it for Monotarou
This review is about item#2212323.
Used for main body moving parts of sealer

From Japan
On 2017-01-24 09:04:42
Just by moving it is that there are many troubles of rotating parts If things can improve the rotation part a little more?
This review is about item#2212332.
Used on the foot of a folding working desk

From Japan
On 2015-10-13 15:08:13
In order to move the work table, the foot adjuster was changed to a free car, easy to change and the burden on the move was alleviated. It is more convenient if there is a wrench for installation.
This review is about item#02212314.
For moving the instrument platform

From Japan
On 2013-05-09 12:02:14
I think that both wheel condition, plating condition, rotation condition, and rolling condition are superior to those of other companies
This review is about item#02212332.
Used for belt sealer and Fuji impulse sealer stand

From Japan
On 2012-11-28 17:18:25
Very well accepted Whether washers, springs, nuts, and set sale are considered also in the future Is it necessarily necessary?
This review is about item#02212323.
Exchange handheld casters

From Japan
On 2012-03-16 14:55:03
Since it is a manufacturer since long ago, there is no problem with quality. It would be nice if you could have attached lock nut (M12) after adjustment if possible.
This review is about item#02212314.
It is attached to the feet of the workbench inside the factory together with the washer.

From Japan
On 2012-03-12 14:51:52
It is enough as it is now
This review is about item#02212305.
I use it so that you can move the handmade loading platform quickly.

From Japan
On 2012-01-26 13:21:28
Both load bearing and smoothness of bearing rotation are satisfactory.
This review is about item#02212332.
1
Customers Who Viewed This Item Also Bought
<<
>>
Screw Type 415EA Swivel Caster, Iron Sheet Wheel, Rubbered Wheel, with Brake
HAMMER CASTER
12.99 - 31.99 SGD
Screw Type 415EA Swivel Caster, Nylon Wheel Urethane Rolling Wheel, With A Stopper
HAMMER CASTER
6.99 - 26.99 SGD