Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Spiral fluted tap (for stainless steel)

Spiral fluted tap (for stainless steel)
Sales Price: 9.99 SGD
Review Rating: 3.60
10 Customer Reviews
5 star 3
4 star 4
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Precision machinery
4
From Japan
On 2015-12-22 20:07:04
Alright
This review is about item#08151105.
Tap work
1
From Japan
On 2013-07-22 22:02:35
Even though it is for a blind hole, an ordinary sparal tap came in. How do you like it?
This review is about item#06299666.
For metal processing
3
From Japan
On 2013-07-22 21:34:46
The cut aji is good, but because it is said to be made in Korea, durability is a bit uneasy.
This review is about item#06299657.
SUS 304 bag tap
1
From Japan
On 2013-05-29 16:15:55
It is the lowest. Tap made in Korea was such a thing. What is for stainless steel! I can not cut it at all. I threw it away. I will not buy it again. It's still worse than made in Japan 50 years ago. Do not sell MonotaRO something like this.
This review is about item#06299641.
Tap to SUS 304
5
From Japan
On 2013-05-21 14:12:10
Used for tapping into the through hole of SUS 304 round bar. It is also influenced by the tangle of the facet and the size of the pilot hole (it is made slightly larger), but I thought that this tap was the most durable. Although it broke up to 950 pieces at maximum, we have exchanged 700 to 750 pieces as a guide. For your information…
This review is about item#08151026.
Blind hole tap M2.3 * 4 places φ 70 mm flange processed to short side
4
From Japan
On 2012-08-15 10:03:05
There is no problem in terms of quality, such as discharge of chips. Pricing is also ordinary If delivery is overdue, if we can deal with delivery date a bit more, or if we can either price setting, continue purchase ...
This review is about item#08151035.
Ss 400 stainless steel tap work
5
From Japan
On 2012-02-11 13:31:53
As expected it is OSG It is satisfactory as expected Although the price is satisfactory as expected The material processed was around 15 mm in thickness All the threads finished cleanly Neither machine nor manual work was able to work smoothly
This review is about item#08151184.
S45C · SUS · SS41 and other material used for lathes and female threads in tapping machines.
5
From Japan
On 2011-12-08 17:41:49
It is what OSG produces in South Korea, but the material is high and sharp. Hold, you can go there so much. Speaking of greed, I think that it is better to cut chips better if the screw part of the tap is a bit shorter.
This review is about item#06299666.
Used for 6 mm shaft center securing screw
4
From Japan
On 2011-10-02 20:55:12
Up to now 3 mm and below were easy to break and thought quite disgusting but I think I found a good thing a little value will be chosen But how many times can we withstand use
This review is about item#06299632.
Tap the stainless steel casting (SUS 304).
4
From Japan
On 2011-02-22 11:45:05
I felt quite nice and it ran out.
This review is about item#06299675.
1