Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Snap Ring for Holes, Steel for Springs, Hrc 44-53,

Snap Ring for Holes, Steel for Springs, Hrc 44-53,
Sales Price: 4.99 SGD
Review Rating: 4.00
13 Customer Reviews
5 star 7
4 star 1
3 star 4
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
As a snap ring
3
From Japan
On 2017-03-24 17:17:08
There is no problem as a snap ring. We will also purchase
This review is about item#5628497.
Used for RC def
3
From Japan
On 2016-04-06 17:06:09
The hole was not small in size, and it did not pass with the KWT tool I used to date. I was putting in and out the same 8 mm snap ring. I was forced to buy Knipex's tool. Even so, the meat near the hole is thin. I am worried about the strength only at the thrust bearings used.
This review is about item#05628357.
For overhaul
5
From Japan
On 2015-12-19 19:17:05
It is convinced with refreshing new article exchange. The price is also cheap and can be used normally. It is even better if there are few more lots.
This review is about item#05628472.
To maintenance
5
From Japan
On 2015-12-10 21:15:40
It was a good item.
This review is about item#05628542.
I tried to use it for a linear bush
1
From Japan
On 2015-02-01 15:57:28
I bought it as a part to be fitted in the groove of the linear bush, but if it spreads it will be damaged so if you check with your company it was a completely different product. Era of ignorance of human beings to buy the net, I wish us a little more clearly. The remaining 53 pieces can not be used. (Oh waste.)
This review is about item#05628393.
To a motorcycle
4
From Japan
On 2013-07-25 13:12:39
I use it for the wheel bearing of the motorcycle
This review is about item#05628542.
Equipment maintenance
5
From Japan
On 2013-01-05 12:36:37
Although it is Osaka soul brand, it was confirmed that the manufacturer could confirm with the product photograph, so I could buy it with confidence. When the pliers hole cracks, it is a part that becomes difficult to remove, so I will search with quality emphasis rather than price, but the price was also cheaper than other brands and satisfactory goods. As PB, I think that there are times when manufacturers may change, but I would like to disclose information to consumers even a little.
This review is about item#05628524.
Agricultural equipment repair
5
From Japan
On 2012-09-13 23:55:33
The strength of the spring is optimum, and there is no deformation even when tightened with a snap ring pliers during installation. Also, even if you hit with a driver for driving, there is hardness that does not get scratched, so it is very easy to work and there is a sense of security.
This review is about item#05628567.
Machine parts installation work
5
From Japan
On 2012-07-12 13:07:36
I used it normally.
This review is about item#05628533.
As a part for experiment.
3
From Japan
On 2012-06-30 23:36:21
If the dimension (d 0, the diameter of the smaller hole) is R-8, it is written as 1.2 mm, but it seems that it is close to 1 mm as measured by scanning. Because I bought it for the purpose of experiment which is not the original usage way personally, I've used the satisfaction level normally.
This review is about item#05628357.
To motorcycles.
3
From Japan
On 2012-06-06 13:55:53
Only one was necessary, but since it was only 30 pieces, it purchased without any help. I'd be happy to have a set of 5 or so, if possible, if there are a little more lots.
This review is about item#05628481.
Restoring old motorcycle etc
5
From Japan
On 2011-04-21 12:23:57
It was saved because I was in trouble because I forgot something when disassembling the engine.
This review is about item#05628542.
Machine repair
5
From Japan
On 2010-04-22 22:58:00
It is convenient to purchase in small amounts when you need it. Goods are also of sufficient quality.
This review is about item#05628585.
1