Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Carbide stainless steel hole cutter (with carbide chips)

Carbide stainless steel hole cutter (with carbide chips)
Sales Price: 39.99 SGD
Review Rating: 3.91
11 Customer Reviews
5 star 6
4 star 1
3 star 2
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 11 of 11 Reviews
Normal use
5
From Japan
On 2017-07-02 17:17:38
The same thing was cheaper than the nearby home center by 1000 yen, Is the home center high or MonotaRO easy? Thank you.
This review is about item#2458233.
Drilling of stainless steel plate
3
From Japan
On 2017-02-16 10:07:12
The price is cheap and very helpful. It is a product I'd like to ask in the future.
This review is about item#2458233.
Drilling of kitchen stainless sink
5
From Japan
On 2016-07-01 22:20:16
This is good, others do not think.
This review is about item#02458233.
Foolishly
3
From Japan
On 2016-03-16 00:44:47
no doubt
This review is about item#02458154.
Drilling of stainless steel box
4
From Japan
On 2015-09-16 16:48:19
At the beginning, the drilling proceeded smoothly, but suddenly the sharpness fell off at 12.3 points, the hole did not open and the color of the stainless steel side changed in the inside so that once stopped drilling and replaced We restarted in Holso. By the way, the stainless steel plate thickness is about 2 mm. The tool I used is Panasonic's charging drill. I thought that it could be used a little more, so it was nice to have prepared the second one. Today, I ordered additional additions.
This review is about item#02458172.
Expansion of watch case
5
From Japan
On 2015-05-18 16:19:34
I'm out of stock. Would it be nice if it was 0.5 mm if possible?
This review is about item#02458303.
Used for drilling in electric construction work boxes etc.
5
From Japan
On 2015-05-04 22:08:29
Shaft and Holesau {edge] part sold separately. I want something that extends the shaft {about 100 mm}.
This review is about item#02458154.
Electrical construction
5
From Japan
On 2013-07-18 13:15:43
Because I was cheap, I was wondering if I could not cut it much, but I think that sharpness is good for the price. I am satisfied.
This review is about item#02458303.
A lot of drilling work on stainless steel plate
2
From Japan
On 2011-09-28 13:01:53
2 purchase 2nd hole can not finish after opening 2 holes
This review is about item#02458233.
Drilling operation
5
From Japan
On 2011-04-06 18:26:43
You may have strong teeth, but it's better if you have a little more depth. I would not say if the price is a bit cheaper
This review is about item#02458233.
Control panel processing.
1
From Japan
On 2010-11-02 22:31:26
All the teeth flew away in about 60 holes. I used the company's products before, but I could use it for a year, I liked it for a long time. I use the same drill. The same plate pressure is unknown. Next we will make other goods.
This review is about item#02458172.
1