Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Carbide stainless steel hole cutter (with carbide chips)

Carbide stainless steel hole cutter (with carbide chips)
Sales Price: 48.89 SGD
Review Rating: 4.62
8 Customer Reviews
5 star 5
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews .
DIY jig creation
4
From Japan
On 2017-05-17 18:42:45
I used it for drilling a 5 mm thick stainless steel plate. It seems that it is a little thick, I felt 3 mm thick is appropriate.
This review is about item#2458321.
Drilling to stainless steel door
5
From Japan
On 2016-10-25 16:42:27
There are only famous manufacturer items and sharpness is good. I think that the center drill is a little long.
This review is about item#2458382.
Drilling of steel material (4.5 mm)
5
From Japan
On 2015-07-08 20:44:59
I opened holes in 10 square shaped steel materials, but it seems likely that the hole saw is still going, I wonder if the center drill has run out. I bought one for spare but it seems to be useless for a while.
This review is about item#02458355.
Electrical construction
5
From Japan
On 2013-07-18 13:11:01
Because the price was cheap, I was wondering if I could not cut it much, but I am satisfied with the sharpness also for the price.
This review is about item#02458355.
I installed a hole in the stainless steel top board to attach the alkaline ion water conditioner to the sink.
4
From Japan
On 2012-05-02 14:52:40
I could drill without difficulty. Speaking of greed, it was the best if there was enough depth to drill a reinforced plate under the stainless steel plate together. I could not penetrate because the upper side of the cutter was wider.
This review is about item#02458434.
Perforation of 2 mm stainless steel plate
5
From Japan
On 2010-10-04 16:09:30
In the drilling of 2 mm stainless steel plate, it is difficult for inexpensive carbide cutters and bimetals to be inadequate, and again it is difficult unless it is of this class. As expected there are only maker items, it is expensive but it will expire well.
This review is about item#02458321.
Drilling
4
From Japan
On 2010-06-21 08:18:08
good
This review is about item#02458382.
Drilling of stainless steel plate
5
From Japan
On 2010-01-30 14:54:31
It is outstanding sharpness that there are only maker items. Even cemented carbide is a stainless steel opponent and it can be used only a few times, so it will be nice to be a bit cheaper.
This review is about item#02458452.
1