Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Concrete drill Insert top bit (SDS-plus) TT type

Concrete drill Insert top bit (SDS-plus) TT type
Sales Price: 8.99 SGD
Review Rating: 4.11
18 Customer Reviews
5 star 7
4 star 7
3 star 3
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 18 of 18 Reviews
Three minutes anchor pilot in electrical work
5
From Japan
On 2017-11-08 18:28:38
I used 12.5 Φ as a pilot hole of a 3-minute anchor. In case We have opened 300 to 400 pieces in a short period of time, I survived enough In the last direction, the animal was not able to enter the animal, but I am satisfied as the amount of work.
This review is about item#2276872.
When concrete drilling
5
From Japan
On 2017-09-16 15:56:13
I bought it as stock. It is handy when drilling.
This review is about item#10041981.
Work of attaching steel bundle to concrete soil
2
From Japan
On 2017-05-27 06:04:01
Although the cutting edge of the tip is satisfactory, the mandrel shaft is soft, and it is bent by just slightly tilting the drill, the vibration drill grinds. I would like you to make it with a little harder steel.
This review is about item#2276942.
Drilling
4
From Japan
On 2016-11-04 16:56:42
Normally you can speed up the drilling quickly, but on the uneven surface Miyanaga is easy to use
This review is about item#2276906.
Anchor bolt driving
5
From Japan
On 2016-10-15 14:35:46
Drilling work is possible in a short time. A hole opens beautifully
This review is about item#2276906.
Construction of post-construction anchors
5
From Japan
On 2016-04-16 15:40:17
I hope the dust will be reduced.
This review is about item#02276845.
Sash mounting
4
From Japan
On 2016-02-10 11:14:59
It is durable.
This review is about item#02277055.
Fixtures
3
From Japan
On 2015-10-05 14:03:11
Normal upper class !!
This review is about item#06684027.
Drilling in concrete
4
From Japan
On 2015-02-12 20:11:34
It may take a while for the tip to collapse. I want you to be a little more robust.
This review is about item#10041981.
Drilling concrete
4
From Japan
On 2013-12-20 18:31:27
I can cut well for the price. If it is a bit cheaper, I should say something.
This review is about item#06684115.
Drilling of concrete surface
3
From Japan
On 2013-10-23 15:26:11
It is not bad, but it will break a lot. Is it not easy to use?
This review is about item#06684002.
Use a viscone to fix the liner on the back wall
5
From Japan
On 2013-07-18 20:29:44
It lasts long and has a long life and sharpness is sustained and convenient.
This review is about item#10041972.
Drilling of anchor bolt
5
From Japan
On 2012-11-06 12:54:52
It is sharp
This review is about item#02276854.
Concrete screw fixing
4
From Japan
On 2012-10-12 12:29:41
It is preeminent workability, making drilling fast.
This review is about item#10042015.
Plumbing fixation
4
From Japan
On 2012-10-04 04:53:23
Although it was used when fixing the piping, it was able to open a considerable number of holes without breaking.
This review is about item#10041997.
Concrete beak
3
From Japan
On 2012-05-23 19:40:02
I could use it without any particular change.
This review is about item#02276845.
I would like to use it for construction of the fence.
4
From Japan
On 2012-04-05 15:59:35
Although I have not used it yet, I will try to use it in a while, if there is no problem, I would like to purchase again.
This review is about item#02276942.
Site water supply and drainage facility construction
5
From Japan
On 2012-03-09 16:26:23
Used with rechargeable hammer drill. The price is also reasonable, if you break a hole without refrain, buy it again. How about a set of bits and non-processable
This review is about item#02276942.
1