Customer Reviews of Ball Grip Screwdriver
The reviews are automatic translation.
Showing 1 - 20 of 70 Reviews
Electric wiring, assembling furniture at home etc.

From Japan
On 2018-04-14 14:53:34
Compared with other drivers, bite to the screw is good, so you can tighten without squashing the threads. Also, since bits are magnetized, it is convenient for screws to stick together. I already bought three for home use, hobby use, work use, but I am very satisfied.
This review is about item#2197492.
Maintenance of oil stove

From Japan
On 2018-04-11 16:12:38
I ordered it because it is the same as the type I have used so far.
This review is about item#2197526.
Machine maintenance, etc.

From Japan
On 2018-04-10 08:48:34
I used it for about 1 year after purchase. You can purchase goods with a length of 30 cm, you can use with confidence without worry of crushing screw threads even without putting too much force on screw detachment.
This review is about item#02197544.
Car maintenance

From Japan
On 2018-03-31 01:00:57
I have been using it for over 10 years, but I am happy that I get the same thing. After all familiar with hands is cheap to use.
This review is about item#02197526.
Working time tightening screws

From Japan
On 2018-03-20 17:30:50
I bought a 6 mm wide one, but I wanted a 7 - 8 mm one if there was one.
It seems to be useful because the tip is a magnet.
Because the grip is large and rubber, the force is put without slipping.
This review is about item#2197587.
General maintenance

From Japan
On 2018-03-10 22:13:22
Cost performance is outstanding. Because it is cheap, it can be used without hesitation even with a slightly rough usage.
This review is about item#2197596.
Bike Maintenance etc.

From Japan
On 2018-02-27 22:15:36
It is easy to use as usual! It is outstanding stability. Ball type grips are comfortable. In a narrow area it may be tough as the grip gets thicker, but all else you can go with this.
This review is about item#2197526.
When replacing motorcycle parts

From Japan
On 2018-02-11 08:35:18
I bought it to take out the screw which I never reached this time. It is safe because it is Bessel item.
This review is about item#36701515.
Electric Works · General maintenance

From Japan
On 2018-02-07 17:52:02
I think the grip is comfortable in hand and it is easy to grasp. I love +2, but I've been using head for many years, but it is really small.
Because this time is the 4th in 45 years, I think that it is perfect for COSPA.
This review is about item#2197526.
Maintenance of two-wheel four-wheel machines, etc.

From Japan
On 2018-02-01 18:27:37
Plus # 3 Driver purchased for trial because there are few things to pick up at the store. According to the label affixed to the shaft it was for the electric work of "for electric terminals". It seems to fit the current 6 mm thread groove, but the grip part is the same size as # 2, so it was too small to loosen the 6 mm screw that was tightened firmly with air / electric tool during production. There is also a hand hanging a big monkey in the dent of the grip part, but I do not like it because it hurts.
This review is about item#38572405.
Daily repair work etc.

From Japan
On 2018-01-18 12:10:54
Compared with the plus ratchet driver I bought at the same time, the grip part is quite small.
I also wrote about that review, my hand is 20 cm from the tip of my thumb to the tip of my little finger, which may be smaller than the recent younger one.
Even so, it feels very small.
This review is about item#2197553.
Maintenance of motorcycle

From Japan
On 2018-01-11 16:23:01
I also liked the color, I think that it is easy to use with kanji that is familiar to the hands
This review is about item#2197517.
It is not fixed work in particular, it is used in every scene.

From Japan
On 2017-12-31 21:12:11
I purchased it because I lost what I was using. I do not think the impression needs to be discussed further. It's a nice thing.
This review is about item#2197587.
Overhaul of motorcycle

From Japan
On 2017-10-07 15:53:36
It is the best item of COSPA
I am doing all this driver
This review is about item#2197544.
Used for machine maintenance.

From Japan
On 2017-08-08 22:00:31
I have been using it for a long time, but it is very easy to use.
I like it a lot.
This review is about item#2197526.
Equipment maintenance time

From Japan
On 2017-07-24 17:54:31
Because it is always used, it will fit in hand. The price is also cheap.
This review is about item#2197535.
Magnetic tip attachment Assembling small screws

From Japan
On 2017-06-10 19:10:57
I seemed to be easy to grasp, I purchased it, I have not used it yet. The admiration also has magnetism and does not screw down.
This review is about item#2197492.
For repairing electric appliances

From Japan
On 2017-04-08 14:51:26
Bessel used other sizes, but it is easier to grasp, so I tried purchasing this size, there is no problem,
This review is about item#2197492.
Normal maintenance work

From Japan
On 2017-03-28 06:58:01
As for the driver of No. 3, since the product was only thick and large, only the goods were found, so I cut off the tip of the old driver of No. 2, welded the bit of No. 3 and used it. I have just found this item and purchased it immediately. It is mainly used for tightening the plus boss of the magnet switch.
This review is about item#38572405.
Screw etc.

From Japan
On 2017-03-16 14:43:29
It is optimal as a regularly used driver and is always in use. Usability is easy to use without problems.
This review is about item#2197535.