Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Double-Sided Neo Lock, With A Blade Latch

Double-Sided Neo Lock, With A Blade Latch
Sales Price: 20.99 SGD
Review Rating: 4.25
8 Customer Reviews
5 star 3
4 star 4
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
measurement
5
From Japan
On 2016-04-05 17:23:54
Although the scale is always used, it will be replaced frequently when bent or dirty, but this product is easy to use, there is a back scale, we are satisfied. I purchase it every time. I purchased about 40 items, including purchases from other stores.
This review is about item#02009156.
Used for measuring products
4
From Japan
On 2016-02-08 14:53:15
It's a little smaller and a little easier.
This review is about item#06069016.
We measure the length of steel and other products
4
From Japan
On 2014-11-07 14:10:54
Slightly loose the metal fitting at the tip. When stretched for a long time, it is easy to bend that part is easy to wear.
This review is about item#05327935.
Building related measurement
3
From Japan
On 2014-01-24 22:54:49
While the width is 25 mm many, as for 19 mm, Koshi is too weak purchase. Although I feel a little heavy, I think it is better than a product with a width of 25 mm. The measurement accuracy is normal. The stopper moves easily.
This review is about item#02009165.
Foundation construction etc.
5
From Japan
On 2013-12-15 00:43:53
In the nearby home center the same thing was over 2000 yen. First purchase 19 mm width. Up to now I was using a thing with a width of 25 mm so how about 19 mm width? I thought, but this 19 mm wide one is felt easier to read. I used both sides before (both sides are made by another company) It is awesome to win. It is convenient to have a shock absorber that was not made by another company. Tape return is fast and can be rewound while adjusting with shock absorber. Even such a function is really useful. Majority etc are used severely in the work of civil engineering, so I have not used the same thing for one year until now. Although I bought a scale equivalent scale if I want a desire, I think that it was better if the back side was not a graduated scale and it was a meter scale.
This review is about item#05327953.
mounting
4
From Japan
On 2013-04-30 10:56:58
Easy to use
This review is about item#05327953.
Measurement of the walls of rooms - inter-wall and ceiling-floor measurements
4
From Japan
On 2012-05-27 07:05:18
Purchased 5.5 m 25 mm. I used the back side for the first time, it is very convenient. Since I have just started using it, I do not know the strength of the back side that tends to rub.
This review is about item#02009174.
It is convenient because memory is on the back side.
5
From Japan
On 2011-05-23 13:38:36
It is easiest to measure up to 5.5 m so I always carry around, but it is shocking that the nearby home center was cheaper ━ ('· c _ · `;) ┌
This review is about item#02009156.
1
Customer Who Viewed This Item Also Viewed
G Lock, With A Blister Pack
Measuring Tape, Stainless Steel
Tape Measure
Spur gear MP equal 1.0
Measure Tape, Double Faces Scale
Lock 22
Chalk Line Reel
Double-faced Measuring Tape