Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Adjustable reamer

Adjustable reamer
Sales Price: 87.99 SGD
Review Rating: 4.11
9 Customer Reviews
5 star 5
4 star 2
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Inner diameter adjustment of insert part of pipe-like parts (bicycle, automobile).
4
From Japan
On 2018-05-09 18:24:37
Aluminum parts are the main processing targets, but in a certain sense "too much", gouge Too good things, things with poor hole accuracy (things that do not have a perfect circle), the initial familiarity I did not cut until I got out. The finished surface is fluffy "made in Japan", there was no wasteful return, and adjustment of dimensions was easy. Variable type was used for the first time, but if this is the case (this product) enough accuracy can be outputted, so the number of tools can be reduced, so it seems to be useful.
This review is about item#6150916.
When you want to increase the hole size a little, when you drop the paint inside the hole
5
From Japan
On 2015-05-29 14:58:24
I bought 16 mm this time and used it. I could buy it immediately in time, I could finish my work without troubling the final customer. The finished state was also satisfactory.
This review is about item#06150864.
Hole drilling of connecting rod
5
From Japan
On 2015-05-09 08:48:38
It was very easy to use.
This review is about item#06150855.
Cutting of metal
1
From Japan
On 2014-09-26 16:17:04
I can not cut at all. It is a defective product.
This review is about item#06150855.
For finishing after hole drilling
3
From Japan
On 2014-08-27 19:51:18
Easy to use because it can delicately adjust the inner diameter.
This review is about item#06150873.
Hole correction
5
From Japan
On 2014-06-22 14:49:44
It was very good.
This review is about item#06150846.
Bicycle seat tube processing
5
From Japan
On 2013-10-03 11:21:09
I used it for the expansion of the seat tube of the chromoly frame It was supposed to be 27 mm in dimensions, but it looked like it could cut from 26.8 mm with a caliper, so I used it immediately with a 26.8 mm seat tube without problem 26. Since 8 mm was able to shed, we could gradually increase the size and expand it to 27.2 mm. Cutting while changing the dimension about 5 times It was possible to cut the sheet tube neatly with good sharpness
This review is about item#06150925.
Tolerance adjustment of shaft hole
4
From Japan
On 2013-03-21 15:05:32
Because of a brand new, I feel that the adjustment screws are hard
This review is about item#06150855.
Adjustment of gun parts
5
From Japan
On 2012-12-13 22:58:35
This time it was used as a dust cover around the gas piston of the gun to process and adjust the inner diameter of a commercially available aluminum pipe. The adjusterable reamer I purchased before used to adjust the choke size of the muzzle part of the shotgun. I like the point that it's easy to fine-tune the dimensions.
This review is about item#06150855.
1
Customer Who Viewed This Item Also Viewed
Tap handle
Hand reamer
Hand reamer
Adjustable reamer
Spiral Blade Chucking Reamer
Iron Tap Handle
Hand reamer
Hand Reamer
Hand Reamer