Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Three-Way-Type Joint Coupling, With Plating,

Three-Way-Type Joint Coupling, With Plating,
Sales Price: 4.99 SGD
Review Rating: 4.50
10 Customer Reviews
5 star 8
4 star 0
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Air pipe etc.
5
From Japan
On 2018-01-16 08:16:09
I planned to use it for branching of the heater hose but plan changed and I did not use this time but I will use it for air piping again.
This review is about item#05820342.
To the branching of the air hose
5
From Japan
On 2017-12-01 19:30:42
I can use it firmly. Because the hose band is so plainly high, I'd appreciate it if you set sale etc ...
This review is about item#5820333.
Air piping
5
From Japan
On 2017-11-09 16:19:33
Three or bamboo shoots of other companies forced the screws to screw a thin hose and air leaked. I am satisfied because I do not leak this three or one piece.
This review is about item#5820324.
It was used for distribution of gas hose.
2
From Japan
On 2017-07-04 17:15:55
Since the angles in three directions are the same, there were things that narrowed the angle in two directions.
This review is about item#5820324.
Car Heater on Bypass
5
From Japan
On 2017-03-20 08:59:56
I use it as a heater bybas which does not enter the hand of an old car
This review is about item#05820351.
Kerosene piping
5
From Japan
On 2015-11-24 18:10:55
It was good because the quality was well done and the price was easy.
This review is about item#05820333.
Size was wrong ...
5
From Japan
On 2014-10-12 22:28:33
Because it was unexpectedly high in the home center, I bought other parts together, but I bought one smaller size with confirmation mistake in the drawing. The making itself is smart, I am very thankful that these small items can be purchased cheaply.
This review is about item#05820367.
Adjustment of motorcycle cab
5
From Japan
On 2014-01-14 23:33:43
It is used to branch the hose from the adjustment sub tank by adjusting the FCR carburetor with two fuel hoses. I chose because the price is also cheap and made of metal and durability seems no problem. The gasoline flow rate is also insufficient, I am satisfied.
This review is about item#05820367.
Hose connection
3
From Japan
On 2013-01-20 12:09:20
When searching, I felt like three, three, three, three, three, three, three, or three ..., even if I knew the shape, I did not know the name but it was hard to find it if there was originally a pre. (I arrived after following the purchase of surrounding purchase)
This review is about item#05820324.
A joint
5
From Japan
On 2011-05-28 22:26:30
Even at home centers this kind is not complete. However, such abundance is indispensable in the field. From here on out, please do your best. I support you.
This review is about item#05820333.
1
Customer Who Viewed This Item Also Viewed
Hose Nipple
T-Shaped Hose Nipple
3 Way Hose Joint
Y Hose Joint 1/4
T Hose Coupling
Three-way hose joint
Three-way Joint Hose
Three-way hose joint
Y Type Contact Hand
Three-pronged direct connection fittings
Three-pronged hose fitting
Mitsuwanta Housros NO.14
Y Hose Coupling
T Hose Coupling