Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Ring Joint

Ring Joint
Sales Price: 2.99 SGD
Review Rating: 4.33
18 Customer Reviews
5 star 11
4 star 2
3 star 5
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 18 of 18 Reviews
machine
5
From Japan
On 2018-06-16 17:37:05
I think that it is very good product and excellent in cost performance.
This review is about item#5820823.
It is used for an air tank.
5
From Japan
On 2018-04-16 18:08:32
Some stores are cheaper than others, and some are expensive. There are many things with short delivery times, but there are also very long ones. I use it properly.
This review is about item#5820875.
Water piping end
5
From Japan
On 2018-03-04 18:55:22
It is used for edge cutting of water piping which became unnecessary. I tried using it because it was a difficult place to solder under the floor. Work was easy and it was possible to use without problems.
This review is about item#5820927.
Hot water piping
5
From Japan
On 2018-01-22 16:33:03
Although the ring type is a little expensive, soldering is unnecessary and it was easy to construct. The connection strength of the ring was also sufficient.
This review is about item#5821112.
Air piping
5
From Japan
On 2017-12-05 21:05:02
I misunderstood that sleeve (abacus ball) is not attached, but it was properly attached.
This review is about item#5820805.
Connect to air tank
5
From Japan
On 2017-11-14 16:33:48
It is very cheap and it can purchase it and I am very satisfied without air leakage
This review is about item#5820787.
Kerosene tank piping
4
From Japan
On 2017-03-02 20:42:23
The price was also cheap, very easy to use, work progressed smoothly.
This review is about item#5820954.
Repair
3
From Japan
On 2016-10-19 17:39:28
It does not specify whether a ring ball is attached or not. Result Although it was attached, it is unkind, it is a shame to wish you can write a bit, so that you can purchase without stress. If the item arrival was also a day late, until the return to the house is an excursion, until the product arrives at the user at work?
This review is about item#5820796.
Repair of water heater
5
From Japan
On 2016-07-26 10:01:11
It was urgent, but the next day, it arrived in the morning, so I got the job done soon.
This review is about item#05820927.
Air piping
3
From Japan
On 2016-04-15 15:59:47
It was used for check pipe and copper pipe connection. It can be used normally, there is no particular problem.
This review is about item#05820832.
Oil piping, air piping
5
From Japan
On 2015-10-12 18:22:35
It was good if listed pressure resistance etc. (Checked on the maker homepage, it was 3.45 MPa or less)
This review is about item#05821155.
Water leak test of copper pipe brazed parts
3
From Japan
On 2015-05-12 20:39:32
In terms of piping design, the insertion depth of the copper pipe is necessary for precision piping design. The measurement result was 23.4 mm. I also appreciate G (PF) screws on the mounting screws. Although it is in other companies, it is expensive.
This review is about item#05820927.
Air piping in the garage
3
From Japan
On 2015-03-09 11:52:12
I purchased it by mistake in size but it was a mistake order from my misunderstanding. The size table at the time of ordering was easy to see. It is saved because many products with attractive prices are prepared. Thank you for your next opportunity.
This review is about item#05820866.
Pipe repair accompanied by hot water type ceiling embedded bathroom dryer replacement
5
From Japan
On 2015-01-30 20:00:18
Existing bathroom dryer was piped by 8φ copper tube brazing and we tried to repair too because the back of the ceiling was so narrow that we could not braze work so we used this product. There was no leakage and piping could be done without brazing
This review is about item#05821121.
Piping work of home tank
4
From Japan
On 2015-01-19 15:42:37
Although some of the oil leakage was confirmed after installing in the past, it seems that it got better whether there was improvement of the ring.
This review is about item#05820884.
Connection of existing copper pipe
3
From Japan
On 2014-11-14 22:53:05
Is the ring nut size 21 mm? I wish it was a normal spanner size.
This review is about item#05820875.
Grease piping of blower
5
From Japan
On 2012-04-25 12:51:31
It can be used as usual. The refrigerant pipe is used as a grease pipe and it is used as a connecting metal. If you prepare more various hardware, variations will spread and it will be saved.
This review is about item#05820832.
NC lathe cutting oil joint
5
From Japan
On 2010-09-23 22:13:52
Because the six corners are wide, you can strongly fix the pipe!
This review is about item#05820805.
1