Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of JETBROACH Cutter, One Touch

JETBROACH Cutter, One Touch
Sales Price: 109.99 SGD
Review Rating: 4.11
9 Customer Reviews
5 star 5
4 star 2
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Drilling
5
From Japan
On 2017-11-24 17:53:30
Although it was an additional purchase, it was delivered on the day, so it was saved soon for the work in a hurry
This review is about item#2155027.
Drilling into steel frame
4
From Japan
On 2017-09-28 15:40:12
It's neither good nor bad. I can use it normally. I wish the delivery date was a little earlier.
This review is about item#2154923.
Steel bolt connection hole drilling
5
From Japan
On 2016-10-19 17:26:15
I have used it for many years. Sharpness is good, long lasting item. I am very satisfied with Monotauro prices as well.
This review is about item#2154966.
H Hole drilling
1
From Japan
On 2016-08-16 15:32:12
It has become impossible to cut by only 10 holes drilling work. Is there a problem with durability? Or is it a bad product?
This review is about item#2154966.
Used to drill steel
5
From Japan
On 2016-06-11 04:34:23
It was a big success
This review is about item#02154923.
Drilling work of 30 mm iron plate
5
From Japan
On 2016-01-04 12:47:00
Very cheap
This review is about item#07000147.
Hole drilling of corner pipe of 150 angles or more which is difficult to correspond mainly to mold and laser
3
From Japan
On 2015-05-05 10:06:25
Is it really pricing licking users in Japan? Is the manufacturer abandoning the Japanese market? Do you intend not to make it in Japan? It is a complaint from the hard user of Nitto Kohki.
This review is about item#02154905.
Drilling of iron plate
5
From Japan
On 2015-04-29 15:05:50
Since it is an iron plate, it may not be so long.
This review is about item#02155815.
Steel material processing for electric construction materials
4
From Japan
On 2014-09-24 13:38:59
The usual materials can be drilled quickly without problems and work can be carried without carrying materials, so the burden on the workers is small. However, there are variations in the hardness among ordinary steels, and even when not cutting at the beginning of cutting is there
This review is about item#02154941.
1
Customer Who Viewed This Item Also Viewed
Deltagon metal bowler 350A
JETBROACH Cutter, One Touch
Pilot Pin, Centering
Broach holder
Pilot Pin, Centering
Pilot Pin, Centering
Mini Broach
Delta gon metal borer 500 A
Sleeve Ass'y
Jet brooch
HIBROACH Cutter, One Touch
Drilling Unit, Atra Ace
Atraace