Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Oil Pot Window, Screw Stop Type

Oil Pot Window, Screw Stop Type
Sales Price: 13.99 SGD
Review Rating: 2.33
3 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Used for mechanical repair parts
From Japan
On 2017-03-13 15:48:28
It was saved because old machine parts used for maintenance of old machines matched and I would like to ask again in the future.
This review is about item#2040394.
The oil leakage occurred from the oil gauge of the oil machine of the press machine, and it was replaced.
From Japan
On 2017-01-05 16:01:28
I installed the pot windows I purchased earlier, but because the oil leaked soon I bought two extra this time, when looking good after opening it has cracks from the mounting hole and the outer diameter is also half cracked It was. Since it seems that it seems okay if I examine the remainder, I think that it will not be possible to return the amount that is split because it seems okay, so I made it as a sample of the drilling. I think that the manufacturer also wants thorough inspections when shipping. I thought that it was broken that I installed the first time now.
This review is about item#2040394.
Metal saw cutting oil window
From Japan
On 2012-06-19 16:52:03
Although the transparent part may be strong and strong, on the other hand, the white reflection part is too brittle than I imagined. There will be aged deterioration, and how about trying to think about the material of the reflective part as well? There is a possibility of lot-out, so I will only buy it again.
This review is about item#02040394.
Customer Who Viewed This Item Also Viewed
Oil Pot Window, Permanent Type
Oil Pot Window, Permanent Type
Oil Pot Sight Glass Nozzle Type
Oil Level Indicator
Oil pot window HL type
Oil Pot Window
Oil Cap
Breather Cap
Oil Level Indicator
S-shaped oil gauge
SM type oil gauge