Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of New tap metric thread screws

New tap metric thread screws
Sales Price: 8.99 SGD
Review Rating: 4.20
10 Customer Reviews
5 star 6
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Tap processing
3
From Japan
On 2018-03-27 16:24:49
Since the goods themselves are YAMAWA, there is no problem, but there is a problem with the way Taro Taro sends out. I bought ten M4, M3 and M2 taps this time, but I just put it in a bag, but I just put in it, so after arrival, it all got out of the subdivision bag and mixed up.
This review is about item#4546175.
Car Maintenance
5
From Japan
On 2016-10-20 18:55:59
Rusted female thread is beautiful and satisfied.
This review is about item#8166724.
Tap processing
4
From Japan
On 2016-05-23 16:23:15
You can cut cleanly with very little power. The strength is weak.
This review is about item#04546595.
Simple resin material processing
5
From Japan
On 2016-03-14 14:45:50
I was able to proceed without any problems in processing to a resin material.
This review is about item#08166681.
For manufacturing optical benches such as Sigma optics
5
From Japan
On 2016-01-31 20:17:08
I think whether anything can be used for tapping M16X1, but we used this tap for tapping M16 which is open to optical benches such as Sigma optics. Later talk: When asked with chat support, M6 (!) Was introduced by facsimile afterwards, but this is what I wanted.
This review is about item#08166767.
Used for simultaneous biaxial tapping process of brass and curable resin
2
From Japan
On 2015-10-23 18:37:48
We are using it for tapping process with 2 axes at the same time to brass inserted in thermosetting product. Because the product hole is stopped, the tap tip is used by scraping it flat. The one I bought this time was for the second tap so I will consider raising taps next time. Furthermore we catalog. Raising tap product verification was not possible.
This review is about item#04546394.
M12X1, 25 tapping screw
5
From Japan
On 2015-08-11 06:41:17
The screw part of the nut was corrected with M12X 1, 25 tap (YAMAWA). Very sharp. Although the price side is a little expensive, I would like to use other sizes.
This review is about item#08166724.
S45c
3
From Japan
On 2015-02-20 21:56:41
There is neither good nor bad for processing by a single item
This review is about item#08166715.
Tapping of aluminum servo horn
5
From Japan
On 2014-05-13 19:34:28
High accuracy tapping is possible. M2.5 is thin so be careful not to break, so be careful.
This review is about item#37650523.
Screw faced assembly work during staircase production
5
From Japan
On 2012-02-19 12:46:37
I also used taps from other companies, but the tap of Yamawa is very satisfied without a break even though it has a long life. It is truly a Yamawar. I think that work also goes up and cost performance is also excellent as a result.
This review is about item#04546595.
1