Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Chain Lever YII

Chain Lever YII
Sales Price: 99.99 SGD
Review Rating: 4.46
13 Customer Reviews
5 star 10
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
Unfortunately I could not use it
1
From Japan
On 2017-12-31 16:14:42
I was wrongly careless, but since the picture is the main body of the lever block, I did not think it would come true just a lever. Could you just leave the photo for the lever
This review is about item#2131692.
Installation of steel materials at high altitudes
5
From Japan
On 2017-01-30 18:59:47
Used for prevention of material drop at high places, for safety measures. Since installation adjustment can be done with one hand, we were able to work with peace of mind.
This review is about item#2131771.
Heavy machine Tseng wearing
5
From Japan
On 2016-12-03 15:34:07
The body is reasonable in size, light in weight, easy to handle.
This review is about item#2131762.
Lift a heavy thing outdoors using three fangs. It seems to be able to do a reliable lifting that can not fail.
5
From Japan
On 2016-08-13 18:45:36
Those of the same type that are considered for business use are expensive, so it is appreciative that it is affordable.
This review is about item#2131771.
Car engine replacement etc.
5
From Japan
On 2016-01-13 16:24:23
Since it is a maker product, there are no problems such as reliability, ease of use and so on. It is a thankful place for monotalou to get it immediately.
This review is about item#02131771.
Load tightening work of light tiger
5
From Japan
On 2014-01-23 16:35:40
Very easy to use. It is compact and easy to work. There is not much. Because I liked it, I repurchased multiple items of the same thing and size.
This review is about item#02131762.
Prevents detachment of PVC tube adhesion.
5
From Japan
On 2013-12-03 21:12:39
Because it is light, it is easy to take it over the existing ceiling. I think that it is very easy to use. The best attraction is cost performance! It is!
This review is about item#02131771.
Connection of large-diameter PVC pipe
5
From Japan
On 2013-09-25 12:02:42
It was small and very good product. I think that the price was reasonable and very good.
This review is about item#02131762.
Use it temporarily when hanging piping etc, hanging it, lifting a machine part a little, etc.
4
From Japan
On 2013-04-14 15:16:22
It's lightweight and unexpectedly good to use. However, it seems better to have a thicker grip on the arm a little more.
This review is about item#02131771.
Repair of inclination of vinyl house
3
From Japan
On 2012-07-07 12:25:50
I bought a friend's stuff and used it very conveniently, so I bought the same product. It is a compact and very useful tool.
This review is about item#02131771.
Loading up in mountains
5
From Japan
On 2012-07-01 20:09:28
It is lighter and can be unloaded up to 150 kg and it is a good trip.
This review is about item#02131771.
Piping work packing Other
5
From Japan
On 2012-02-27 17:30:54
It is as used before. It is not the first time to use it
This review is about item#02131771.
Used very much like sheet metal work and vehicle fixing
5
From Japan
On 2012-02-03 23:53:13
It is very easy to use and strong.
This review is about item#02131787.
1
Customer Who Viewed This Item Also Viewed
Lever Block L5 Type
Small and Light Chain Block C-21
Lever Block L Type
Lever Hoist YA Type
Super Lever
Hand Power Puller, 1T
Chain Puller
Lever Hoist
Lever Hoist
OH Lever
Lever hoist YAD type (small type)
RN1 series lever hoist
Lever Hoist
Oreck Lever Neo
Lever Block