Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of SA Type Swivel Caster, Double Bearing, Angle Type, With Stopper, Nylon Wheel

SA Type Swivel Caster, Double Bearing, Angle Type, With Stopper, Nylon Wheel
Sales Price: 5.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
On the foot part of the sandblast cabinet
5
From Japan
On 2016-11-10 22:31:37
This caster was very helpful because I did not put it in the home center. Besides, it is very convenient because it can be easily installed in the L-shaped angle of the foot part of the sandblast cabinet.
This review is about item#2540815.
Exchange of BBQ grill casters
5
From Japan
On 2016-08-23 14:56:44
The two legs of the BBQ grill made by USA were stiff and difficult to move and set up at the BBQ party in the courtyard where the two remaining legs were fixed with the wheel not rotatable. So stop cutting the two wheels of the BBQ grill and cut it so that the heights of the four feet are aligned. Cut part Since the sheet metal shape of the foot is 2 mm thick L-shaped metal, the casters purchased inside the metal of this foot are fixed with 4 screws. By all means it became a free leg with a stopper, and the movement and storage of the BBQ grill became easy. Since the load capacity was about half of the allowance, I chose the product, so the movement is smooth and no problem.
This review is about item#2540815.
Required for steel rack
5
From Japan
On 2015-07-06 14:40:47
I bought it to make it easy to move the steel rack. Thanks to the layout change, it will be useful instead of a dolly. In my office, I attach it to all steel racks. However, it can not be said that the delivery date is too long.
This review is about item#02540851.
Workbench
4
From Japan
On 2014-09-29 23:05:45
The movement is light.
This review is about item#02540912.
Mounting on steel shelf
5
From Japan
On 2014-05-30 21:16:27
In order to move the steel shelf, I bought two items that I can lock and two SA-50N. I am satisfied that the nylon wheels are harder to break than rubber wheels with many wheel wear and breakdowns. Those who are concerned about sounds and vibrations while moving think that rubber wheels are good, but if you do not mind, we recommend you here.
This review is about item#02540815.
1