Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of U-Shapped Bolt Set, Stainless Steel

U-Shapped Bolt Set, Stainless Steel
Sales Price: 2.99 SGD
Review Rating: 4.00
3 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Installation parts for balcony power generation
2
From Japan
On 2015-11-27 23:47:42
I felt a sense of incompatibility when I purchased 3 items and saw things that arrived, so when I measured with a caliper, there was quite a difference in size between each part. There were individual differences of 1.4 mm maximum at the tip on the nut side, and there was also a difference in size in other parts. If it says even further, I think that there is a difference of 1 mm or more with the dimensions of the item description page posted, or it may be acceptable within the manufacturing standards but management is not sloppy. I used it because it seems to be used as it is adjusted, but it was disappointing.
This review is about item#06584627.
Setting up product display
5
From Japan
On 2014-04-14 07:30:34
I am satisfied with the quality and the delivery schedule.
This review is about item#03375382.
For clamping clothespins
5
From Japan
On 2013-04-02 13:16:26
Because it does not rust because it is made of stainless steel, it looks better than plated and it does not need to be exchanged.
This review is about item#06584654.
1
Customer Who Viewed This Item Also Viewed
U-Bolts, Stainless Steel
U Bolt, Nut
Open Bolt Set
U-Bolt Set, Iron
Stainless Tube U Bolt
MAME U-Bolt, Stainless Steel
Stainless U-Bolts
Stainless U Band
U-Bolts (Stainless Steel)
SGP U-Bolt
U-Bolts Type A
U Bolt Oval Plate, Stainless Steel
U-Bolt SUS316L