Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Nozzle Five Rs

Nozzle Five Rs
Sales Price: -
Review Rating: 3.00
4 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Planting and planting
1
From Japan
On 2017-06-25 09:41:23
The diameter with the existing hose does not match. I failed. It is possible to use a thick hose of the past.
This review is about item#37670771.
Although it is not a standalone purchase
5
From Japan
On 2016-10-19 22:59:31
As a nozzle with a compact reel. I changed the hose of inner diameter of 7.5 mm recently to 15 mm hose. Since it corresponds, it is natural, but it can be used without problems The pressure and the flow rate have risen considerably and it is satisfactory. I thought about changing to a Petit Progrip garden shower by replacing the hose, but stopped watching the writing that the pressure of STRAIGHT was weak. I spray on motorcycle radiator washing straight, but this is obviously stronger pressure. Frequency is low because it is used only at the time of washing the motorcycle without trouble, but I am using it without trouble for more than 6 years.
This review is about item#37670771.
Watering in the garden
5
From Japan
On 2016-09-30 18:46:27
Both water volume and water pressure are strongly easier to hold and are most recommended for the price.
This review is about item#37670771.
Sprinkling water
1
From Japan
On 2015-06-17 11:26:30
Pistol type lever will not return and will be left unattended. I had one exchanged, but the second one quickly broke down.
This review is about item#37670771.
1
Customer Who Viewed This Item Also Viewed
G Nozzle
Trigger Spray Nozzle
Regular Nozzle
Trigger Spray Nozzle
One Touch Compact Nozzle
Water spray nozzle
Slim Hose Nozzle
Slim Hose Nozzle
Pitter Nozzle G
Takagi smart nozzle N