Customer Reviews of Bi-metal MV
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
To cut material

From Japan
On 2014-07-17 22:21:29
Very well, very much I like it. We will continue to use it in the future.
This review is about item#06631773.
It is used for rough curve cutting at woodworking band saw. Bimetal is not necessary for woodworking, but when stacking 5 to 6 plywood boards and cutting with nails, there is a case where the blade hits the nail in time, so we bought a test.

From Japan
On 2011-02-16 20:35:28
I use ironwork blades for woodworking, but it does not clog and we can cut it to a certain extent. As expected it is long bimetal. Recently Hunaso 's blue can is also handled items, it is cheap and interested. Hunaso is a long-established store in this industry, I think that there is 0.5 mm and 0.36 mm of 0.6 mm or less in thickness. In woodworking, the thinner the blade it cuts. I would like to purchase a coil blade with a blade width of 5 to 6 mm, 8 to 12 mountains per inch, and a blade thickness of 0.5 mm or less. It is good in obtaining goods, so I want you to handle it as a standard handling.
This review is about item#06631755.
Cutting off characters

From Japan
On 2008-03-01 09:41:26
I used other manufacturers, but it is unchanged, economic and nice. It would be nice to have 3 mm.
This review is about item#06631773.
1