Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Normal Hose Grip

Normal Hose Grip
Sales Price: 3.99 SGD
Review Rating: 4.43
14 Customer Reviews
5 star 10
4 star 2
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 14 of 14 Reviews
Vehicle maintenance material
5
From Japan
On 2017-07-10 19:58:28
Although incorrect usage is scattered in the review, this is a general standard of German products and is used for low pressure piping. Suitable for air ducts, low pressure fuel hoses and so on.
This review is about item#5837142.
Installation of agricultural hose
5
From Japan
On 2016-11-18 00:13:48
It is made strong by making it solid. At the time of use, the damage of the thread part is also less.
This review is about item#05837106.
Used during machine repair.
4
From Japan
On 2016-07-28 17:27:23
It is fine as it tightens securely
This review is about item#05837106.
Hose stop
5
From Japan
On 2016-03-16 22:30:03
It can be used without problems.
This review is about item#05837115.
Fixing hose for inflating
5
From Japan
On 2015-10-30 20:48:46
It can be used without problems.
This review is about item#05837106.
Fixing of fuel pipe
3
From Japan
On 2015-09-20 07:30:52
I felt that the screws were small.
This review is about item#05837106.
Air hose
5
From Japan
On 2015-02-03 15:37:49
It is made of stainless steel and easy to use. I think that it was tightened firmly for carbon dioxide gas.
This review is about item#05837106.
Used for connecting Sumirein 50 and Machino coupling
1
From Japan
On 2014-08-25 07:01:23
The width of the band was narrow, and the screw groove was not able to withstand strong tightening and it collapsed. From the conclusion it can not be used for irrigation tubes for agriculture like Sumirein 40 or 50.
This review is about item#05837142.
Hose piping
5
From Japan
On 2014-05-12 18:40:21
There was nothing with problems in particular.
This review is about item#05837124.
Radiator Hose / Heater Hose Relationship
5
From Japan
On 2014-03-28 22:57:46
Although it was only failing in various bands of the manufacturers, this band was able to stop the leakage with the kitchen. You can recommend it.
This review is about item#05837124.
Various uses such as air, water, oil
5
From Japan
On 2014-03-13 18:15:56
I think that it is the best product among similar hose clamps. Making is also solid and the stainless steel to the screws can also be widely trusted for the application. Just because it is more expensive than the home center, I expect to sell bundles such as 10 units.
This review is about item#05837142.
Gasoline hose and radiator hose
4
From Japan
On 2014-03-03 17:48:48
I was worried about whether to withstand the tightening force of the 40 Ø radiator hose, but it seems to be okay.
This review is about item#05837133.
For cars
5
From Japan
On 2013-12-19 19:53:33
It can be concluded without damaging the hose.
This review is about item#05837124.
Motorcycle carburetor insulator tightening
5
From Japan
On 2013-01-30 18:02:09
Only the manufacturer only saw the large size of the tightening part with a narrow width.
This review is about item#05837133.
1