Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Tape Measure

Tape Measure
Sales Price: 24.99 SGD
Review Rating: 4.67
6 Customer Reviews
5 star 5
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Measure cable length
5
From Japan
On 2016-10-18 11:50:26
It is easy to use. Since the lock mechanism is also firm, it will not be unexpectedly rolled up.
This review is about item#5862297.
Wood work
5
From Japan
On 2016-08-29 16:35:00
Cost performance satisfaction problem No point
This review is about item#5862263.
Dimensioning the ceiling
5
From Japan
On 2014-08-18 00:07:54
If it is a one-sided scale it will not break if it hits the ceiling. With this double-sided scale it can be measured about 2 m without breaking. I really like it.
This review is about item#05862236.
Surveying and plotting
5
From Japan
On 2014-06-19 14:07:52
I often use it at the site work, but since it is often used by stepping on the scale itself it will crack immediately. And since the size to use is 10.0 m and so long, the weight of the main body also becomes considerable. It is a sort of thing if it gets a little lighter and it becomes stronger.
This review is about item#05862263.
Measuring
3
From Japan
On 2013-10-24 16:51:13
The price is not much different from local Homsen. Compared with the same product purchased at Houmsen several years ago is it due to cost cutting? I think that the hardware part of the Major had quite thin. If you extend it to measure a long length in the air it will break in the middle. The previous one is a husband that did not have such a thing.
This review is about item#05862236.
Dimension measurement in inspection work
5
From Japan
On 2012-11-23 12:19:57
Width 25 mm Yes hard to break, memory is also on the back side is very convenient.
This review is about item#05862202.
1
Customer Who Viewed This Item Also Viewed
G Lock, With A Blister Pack
Tape Measure
Measuring Tape
Tape Measure
Measure Tape
Tape Measure
Measure Tape
Lock 19, Measuring Tapes
Lock 22