Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Bushing Malleable Cast Pipe Fitting White

Bushing Malleable Cast Pipe Fitting White
Sales Price: 2.99 SGD
Review Rating: 4.68
22 Customer Reviews
5 star 17
4 star 3
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 20 of 22 Reviews
Well pump installation work
5
From Japan
On 2018-03-15 11:14:07
There were many kinds of this part, and it was saved because the necessary size was not achieved even at the home center, although it was difficult.
This review is about item#5705935.
Coolant pump IN, OUT
5
From Japan
On 2017-12-19 17:53:42
I used a bushing made of SUS until now, but because I do not have to worry about rust It was made of cast iron and was enough. Also, I thought that the screw thread was rough if it was made of cast iron, but there was no problem at all.
This review is about item#5705822.
Air compressor piping
3
From Japan
On 2017-08-16 02:48:04
It is cheap but necessary and sufficient. I use it without any problem.
This review is about item#05705856.
When plumbing work and parts replacement
4
From Japan
On 2017-01-20 15:21:04
I am using it because it is worth more than the brand name I was using anytime, there is nothing wrong with it,
This review is about item#5705822.
Fire hydrant piping
5
From Japan
On 2016-11-17 14:57:40
Thank you very much for your prompt response.
This review is about item#5706084.
Compressor piping
5
From Japan
On 2016-10-22 07:02:09
Because it is a size that does not sell to the home center, it is very helpful.
This review is about item#05705831.
Used for piping
4
From Japan
On 2016-06-29 21:10:02
It is made slightly complicated, but there is no problem in use. It is cheap and satisfactory.
This review is about item#05705856.
piping material
5
From Japan
On 2016-06-07 15:57:08
In the home center, it is very good with unavailable size etc.
This review is about item#05706084.
Construction machine
5
From Japan
On 2016-01-12 17:47:57
I am very satisfied.
This review is about item#05705935.
Use for piping "
5
From Japan
On 2015-10-23 20:02:20
The thing does not change, it was good because it was cheap and fast.
This review is about item#05705856.
Electrical equipment wiring
5
From Japan
On 2015-09-23 15:32:01
Cheap price
This review is about item#05705874.
Included in the product as an accessory
4
From Japan
On 2014-12-04 16:20:33
It is easy to use because it is in a bag in units of one.
This review is about item#05705847.
Resizing of hydraulic coupler
5
From Japan
On 2014-07-07 06:26:00
no problem
This review is about item#05705831.
Piping
5
From Japan
On 2014-05-26 23:35:33
I was in a plastic bag. Especially it was able to be used without problems.
This review is about item#05705874.
Use for piping diameter difference fitting.
5
From Japan
On 2014-05-15 09:58:45
I could connect normally by changing piping size.
This review is about item#05705883.
I bought it for plumbing of snow removal.
3
From Japan
On 2014-04-25 13:44:24
Shipping was quick and convenient.
This review is about item#05705944.
For agriculture
5
From Japan
On 2013-11-22 20:43:55
Even cheap, it was a good item.
This review is about item#05705987.
Plumbing work
5
From Japan
On 2013-10-24 15:31:33
It was easy to use.
This review is about item#05705944.
Connection of well pump
5
From Japan
On 2013-08-19 13:33:57
I am not a professional. So, you can purchase it with confidence if you can describe the item description specifically for millimeter to millimeter for connection etc.
This review is about item#05705917.
Air piping
5
From Japan
On 2011-10-25 12:08:17
Even a few can buy it cheaply! There is no problem with thread mountain etc!
This review is about item#05705883.
1 2