Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Countersunk Head Machine Screw, Stainless Steel

Countersunk Head Machine Screw, Stainless Steel
Sales Price: 8.99 SGD
Review Rating: 4.63
68 Customer Reviews
5 star 53
4 star 5
3 star 10
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 20 of 68 Reviews
For repairing electrical parts
3
From Japan
On 2018-04-10 15:45:23
Not much time has passed since using, but it is good and can be used normally.
This review is about item#5508736.
Model production of hobby
5
From Japan
On 2018-04-08 21:17:57
I appreciate early response as I wanted to use it in a hurry.
This review is about item#5508702.
Fastening of electronic equipment
5
From Japan
On 2018-03-09 14:40:58
Although we are using more than 5000 total, we have zero defective products up to now. I think that things are solid. It is handy because it is cheap because it is sold in a small quantity. I plan to use it in the future.
This review is about item#5508325.
As a robot assembly part for education
5
From Japan
On 2018-02-08 15:20:00
The shape of the header, matching with the driver is also OK, the total length is somewhat negative, the edges are just right round with chamfering.
This review is about item#5508264.
Purchased for repairing equipment using small screws.
5
From Japan
On 2018-01-24 15:05:52
There are equipment that uses quite small screws and purchased for repair. The keys of the car are using screws of M2 and have experienced lost, so we are preparing small screws for repair.
This review is about item#5508221.
Repair of dropped screws
5
From Japan
On 2018-01-07 09:50:41
I purchased it for repair because the screw of the equipment dropped out. Quality was superior and price was not high. I would like to purchase again if it is necessary in the future.
This review is about item#5508955.
Used for various self-made work (DIY)
5
From Japan
On 2017-12-23 06:17:32
It is used for parts that dislikes rust etc., and it is mainly used for installation of small switch etc in aluminum case.
This review is about item#05508106.
Fastening of the detachment of the sash
5
From Japan
On 2017-09-27 18:22:51
It was very easy to use. I think that the price was reasonable.
This review is about item#5508386.
The seating surface (dish surface) is solid.
4
From Japan
On 2017-06-06 21:52:24
In the m6 class, the seat surface (dish surface) is wide and steady so that it can be held stably. If you are even seated, the surface will become flat so there is no worry about being caught. However, this type of screw, unlike a train or a train, because the way to measure the length of the screw is different, the screw part will be shorter than the same size of the other screws (below the seat).
This review is about item#5508946.
work
5
From Japan
On 2017-04-28 22:11:15
Items arrived quickly and I am pleased to be in time for work Thank you very much
This review is about item#5508535.
Leg stitch of mount
5
From Japan
On 2017-04-23 19:29:10
When the flat head screw also became M10, it was not sold to the home center so it was inventory and was really saved!
This review is about item#24346568.
Fixing the panel outdoors
5
From Japan
On 2017-02-05 01:28:13
Stainless steel screw was necessary because it was used outdoors, but it was saved because the nearby home center did not have a relatively long 55 mm screw.
This review is about item#05508666.
Material of goods
5
From Japan
On 2016-12-14 15:03:22
It is good because it can be used without problems for cheap. Since the length is finely aligned, it is also good to choose the perfect one. I am always placing orders.
This review is about item#5508377.
Pig catching trap
5
From Japan
On 2016-11-16 18:45:38
Since there are not any numbers anywhere, I can sell it because I can purchase them all at once.
This review is about item#5508562.
It is used at the time of equipment production. Used where you can see.
5
From Japan
On 2016-11-15 15:58:47
The finish is good for the price. I also like the price is low and the amount is large.
This review is about item#5508413.
Thin Plastic
5
From Japan
On 2016-09-29 19:23:53
It was good because the quantity is contained a lot.
This review is about item#5508106.
As a screw of a personal computer
5
From Japan
On 2016-09-29 17:33:49
It is not genuine but it is not smooth but it's enough. Since it is cheaper than the items of other shops even if including shipping costs, I bought it. I am satisfied.
This review is about item#5508221.
assembly
3
From Japan
On 2016-09-29 17:25:46
It is cheaper to purchase from overseas, but buying thought that it would be fine if free shipping.
This review is about item#5508203.
Tool maintenance tool tool creation tool maintenance
5
From Japan
On 2016-07-17 17:11:26
Since 2.6 mm and 30 mm countersunk head screws were not sold to stores, we were able to purchase large quantities and it was saved. Because it is stainless steel, there is strength.
This review is about item#05508343.
Mechanical box of electric gun
5
From Japan
On 2016-06-22 19:49:41
Purchased as a screw for a Ver2 mechanical box of an electric gun. Screws of this size (3 x 18) are very helpful because they can not be obtained at home centers etc.
This review is about item#05508431.