Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flat Washer, Iron / Uni-ChromiumInch Size

Flat Washer, Iron / Uni-ChromiumInch Size
Sales Price: 7.99 SGD
Review Rating: 4.60
10 Customer Reviews
5 star 8
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Used for bolting with woodworking
5
From Japan
On 2017-11-06 18:16:29
It is cheaper than home center, has enough strength and is saved
This review is about item#5530192.
For woodworking work
5
From Japan
On 2017-10-18 15:44:45
Since it was the size I was looking for, I bought it. Especially it is used without inconvenience.
This review is about item#5530244.
Machine maintenance
5
From Japan
On 2017-02-25 06:26:10
As a consumable item, it will be saved as it arrives as soon as it becomes necessary.
This review is about item#05530201.
As a washer
3
From Japan
On 2016-09-22 12:31:48
Why is the inner diameter of 5/16 "(≈ 7.94 mm) flat washer 9.1 mm? Inner diameter larger than 8 mm flat washer!
This review is about item#5530253.
Black and Decker, Earthman's Vibration Buy as OIS Adapter Production Material for Accessory for Vibration Tool.
5
From Japan
On 2013-07-29 17:27:17
Currently ordering knock pins. B & D is perfect for thickness, just a few long holes and knock pins. Although Earthman is thick, it is sufficient to scrape off the knock pin drive and the corner of the regular pentagon of the flange. It is easy because the outer diameter is almost OK and the inner diameter does not have to leave a hole of about 15 mm. Both take into consideration commonality with BOSCH and accessibility of accessories. Although B & D comes with a spacer, I use a knock pin because it seems that any blade slips and loosens by vibration.
This review is about item#05530192.
Air conditioning work
5
From Japan
On 2012-11-21 16:01:37
It is thick and firm.
This review is about item#05530226.
disposable
5
From Japan
On 2012-08-28 21:53:56
It was disposable for wearing it in a magnet, I used to buy it at a home center before, but I found out that I can cut costs and arrived at MonotaRO. Anyway it is cheap and material cost is greatly satisfied with great reduction.
This review is about item#05530253.
With bolt and nut
5
From Japan
On 2012-05-01 11:14:59
no problem
This review is about item#05530226.
Car maintenance
3
From Japan
On 2012-02-23 16:43:37
no problem
This review is about item#05530253.
For each part fixing bolt nut
5
From Japan
On 2011-08-12 23:07:08
no problem.
This review is about item#05530201.
1