Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Reducing Nipple Stainless Steel Made Threaded Pipe Joints, White

Reducing Nipple Stainless Steel Made Threaded Pipe Joints, White
Sales Price: 6.99 SGD
Review Rating: 4.50
8 Customer Reviews
5 star 5
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Outdoor piping
From Japan
On 2017-07-03 23:27:08
Because this size divergent nipple could not be found in the Monotaro PB product, I made it the lowest price. I can use it without problems.
This review is about item#5702094.
Used as suction of painting machine
From Japan
On 2015-07-10 16:21:39
It can be used without trouble even if it is used for lacquer thinner etc. used as paint suction hose for painting machines It is well received by customers because hoses will not become hard even if they are used for 1 or 2 years
This review is about item#05701963.
Used for circulation pump
From Japan
On 2013-11-25 19:13:09
I love it because the hexagonal part of the nipple you wear with a wrench is thin and easy to handle.
This review is about item#05702085.
Kitchen equipment plumbing work
From Japan
On 2012-10-07 21:21:19
I use it for kitchen equipment plumbing work
This review is about item#05702051.
Irrigation work
From Japan
On 2012-06-10 07:47:04
Things not covered by HC are also here, so it was good to look for them without giving up
This review is about item#05702006.
Piping of water and liquid fertilizer
From Japan
On 2012-06-03 22:26:46
Since it is a part to be reconnected at the time of changing the piping, it made a stain and for the time being, because it connects by a coupling, I decided that the surface with rubber on the diaphragm side seemed to be smooth. Although it could be used as it was without leakage, there were slight scratches on the threads cut neatly, so four stars. Of course if made of cast iron I think that there are more scratches and usually more.
This review is about item#05702155.
It is used for pure water piping.
From Japan
On 2012-04-13 13:57:14
Two-quarter diameter difference is very helpful when there is no narrow place or distance. SUS 316 is necessary for the material, but 304 is used because it is not in the current catalog.
This review is about item#05701981.
Used for self-made vacuum defoamer.
From Japan
On 2012-03-28 13:11:58
It is easy to use, it seems to be easy to make things you think.
This review is about item#05701981.