Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Easy Shift Check Ring Plier

Easy Shift Check Ring Plier
Sales Price: 14.99 SGD
Review Rating: 2.86
7 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 1
1 star 3
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
I tried using it for maintenance of heavy equipment
1
From Japan
On 2016-07-16 20:23:06
I tried using it to remove the C ring (closing direction) with a diameter of about 5 cm. Whether the manufacturing of the product was not sturdy and it was distorted or not completely closed, I was struggling a lot. After all, I lost the structure on the C ring and repaired with a hammer but managed to remove one set somehow but it was broken and I threw it away with one use as I do not want to use the next time.
This review is about item#03390536.
Remove clip
1
From Japan
On 2016-05-08 18:34:16
It will be useless as play will come out as you put power. I bought it as though it was convenient, but since it is a delicate and powerful work, let's buy things that fit the size and purpose. It can be wasteful of time and it is not good for mental health as well. Let 's get Konipex' s thing without hesitation.
This review is about item#03390536.
Motorcycle maintenance
5
From Japan
On 2013-12-26 20:27:59
As easy shift, you can easily switch from shaft to hole as you shift the tip. It is very convenient.
This review is about item#03390536.
Inner race decomposition of drive shaft
1
From Japan
On 2013-08-06 22:30:30
I was attracted to shaft / hole combination and purchased. The feeling of grip was also good, but the tip of the tip broke one side by using immediately after purchase. Is it such a thing from the price? I think that strength is necessary a little more.
This review is about item#03390536.
Bike engine O / H
2
From Japan
On 2013-07-08 20:54:22
It is convenient because it is possible to spread and shrink with one, but if you mention one point of difficulty, if the middle screw is unexpectedly protruding and you can use it if it is a narrow place, I would like to improve the protruding part of the screw.
This review is about item#03390536.
Motorcycle maintenance
5
From Japan
On 2012-05-11 00:59:34
I can say that it is also an idea product, I feel confused that the shaft hole switching function is a bit unfamiliar, but it is not easy to use. There is no troubles like the attachment replacement formula. Unexpectedly the strength and rigidity of the tip of the tool was there, so I am very satisfied with this point. Inevitably, in the case of a cheap tool, the tip will often break right away. If the frequency of use is relatively low, the price is also cheap, so I think it's enough. It is a perfect snap ring plier for packing in the limited space of the tool box. I would like a tool of luxury goods if possible, but for the time being I will think (I can always go?) I can go there.
This review is about item#03390536.
Attaching and removing the shaft and hole snap ring
5
From Japan
On 2011-09-07 16:04:35
Since it can switch with one touch, I use it very conveniently.
This review is about item#03390536.
1