Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stopper Of Scale, Without Scale

Stopper Of Scale, Without Scale
Sales Price: 53.99 SGD
Review Rating: 4.86
7 Customer Reviews
5 star 6
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
From Japan
On 2018-01-23 20:46:26
I am using it for buying and scribing for 60 cm. Vernier is also attached, work efficiency got up and it is super convenient. I ordered for 30 cm also with haste.
This review is about item#5848552.
Scribe work etc.
From Japan
On 2016-11-19 13:34:09
I have been using it for a while, but this is the most user friendly. It was cheaper than I thought so purchase decision!
This review is about item#5848543.
It is specified for checking the cut dimensions of paper and wood.
From Japan
On 2014-10-02 17:44:17
Until now I used a digital caliper, but since the atmosphere of the work site is bad, since there are complaints from the scene and it changed to scale stopper this time, who used measurement Even though it will be the same value, it is popular.
This review is about item#05848543.
Dimension measurement of product, work on scriber work
From Japan
On 2014-03-16 21:27:28
I am satisfied with a solid structure more than I thought. There is no looseness between the scale and the stopper main body and the fixing is also certain, and there is no misalignment during use. Vernier part is also thin structure, making it very easy to see. Although the product was good, this time there is a complaint about Mr. Monotaro. Since I ordered two items this time, once I checked, one of the packages in it was broken and the product protruded outside. What was torn is a transparent part, but it is a material which does not easily break, and it is not thought that it broke during delivery even if it thinks about it. I do not know if it was torn at the time of packing, but if you were torn it should definitely know who to pack. However, what was saved was the return of Monotaro afterwards, correspondence of exchange. It was polite and quick, so there was no impact on work. Since I think that I would like to use it from now on, I hope that there will be no such thing in the future.
This review is about item#05848543.
Assembly of precision machinery
From Japan
On 2014-01-08 23:19:14
This is nice. Since there is thickness, it is good to hurt even those with R such as square pipes. Since it can also be used for adjustment of comma addressing, it is utilized in double.
Work of inking with woodworking
From Japan
On 2011-07-28 21:48:52
As the other person wrote, the fixation can be surely made, there is no misalignment. I feel that there is somewhat deviation in what I bought, but it does not get much bitter.
This review is about item#05848552.
Scribe work
From Japan
On 2011-05-26 10:48:38
This was a good shopping. It was expensive and hesitant to purchase, but I purchased it because it is so cheap as it is the same type. Because it is fixed with a spring, it is difficult to slide, and with a vernier it can be dimensioned up to 0.1 mm like a vernier caliper. It is pretty handy.
This review is about item#05848561.
Customer Who Viewed This Item Also Viewed
Stopper Of Scale, With Scale
Stopper For Scale
Scale Caliper
Linear-Scale Silver, Stopper
Measure Tape, LED
Scale Depth
Ruler Stopper
Combination Square
Scribing Gauge standard type
Column Gauge Thickness 33mm
Circular Saw Cutter Ruler