Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of End mill for aluminum

End mill for aluminum
Sales Price: 24.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Cutting of aluminum material
5
From Japan
On 2017-07-29 07:33:38
High cutting speed, work at high feed, but good sharpness. Long-lasting.
This review is about item#06685646.
Aluminum grooving
4
From Japan
On 2015-09-16 12:01:27
2.5 mm for aluminum has not come out from other companies. . . Successfully beautifully Bali is finished neatly but not for aluminum finish cleanly. However, somewhat, the cutting edge about 3 mm broke away. It is not easy to fly this way. Usage prohibited. For steel such as HSS, it is beautiful to slow down the feed and increase the rotation speed. But processing is slower than aluminum.
This review is about item#06685533.
Cutting of aluminum plate
5
From Japan
On 2012-11-21 12:55:50
The cut in the Z direction is good and the sharpness of the blade is good. If you do not make inconsequential cuts, the cutting edge will jump, but I think that if you use it normally, the cutting edge will last a long time. We would like you to add products with a blade diameter of 1.0 mm by all means.
This review is about item#06685515.
Milling
5
From Japan
On 2012-04-14 00:05:17
Basically, it is used when processing aluminum, but the goodness of biting in the longitudinal direction (Z direction) of the hole processing is quite distinctive feature and it is very easy to use though any material is used.
This review is about item#06685646.
Square hole of aluminum panel.
4
From Japan
On 2011-08-26 14:52:38
There was no melt adhesion of chips like a general purpose end mill, and the problem was solved. However, although I really wanted a one with a diameter of 1.0 mm, I did not find it, so it was 1.5 mm.
This review is about item#06685515.
1
Customer Who Viewed This Item Also Viewed
1AL End mill for aluminum
End mill for aluminum
G General Purpose End Mill 2 Blades
Aluminum End Mill
Cemented carbide end mill for aluminum
2Flute DLC Mill
DLC Mill For aluminum