Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of EX Gold drill ( for stainless and mild steel stub) (EX-SUS-GDS)

EX Gold drill ( for stainless  and mild steel stub) (EX-SUS-GDS)
Sales Price: 8.99 SGD
Review Rating: 5.00
2 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Aluminum panel drilling
From Japan
On 2017-10-30 21:00:43
I saw using a cemented carbide drill, but even if I finished with an end mill, the way Bali came out was terrible and I could not be removed. Therefore, I returned to this product. Processing sound is also small, so it seems to be suitable for processing aluminum panel. If it is stiff (super hard) it tends to think that it will last long, but it was wrong. I normally finish with an end mill, so it is finished in a pincad and I do not need worry about deburring.
This review is about item#5594653.
We made knives in groups. I have an exhibition once a year. We made blades with stainless steel and non-stainless steel of 2 mm to 6 mm and finished with handles such as stag and ebony.
From Japan
On 2011-02-23 16:39:30
It is very well cut.
This review is about item#08101992.