Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Zircon Flap Wheel Disk-Nut Fastening Type

Zircon Flap Wheel Disk-Nut Fastening Type
Sales Price: -
Review Rating: 3.43
7 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Polishing of stainless steel products · iron products
5
From Japan
On 2013-09-23 19:20:52
I am glad if there is Φ 180 in MonotaRo product.
This review is about item#07320616.
Flat finish of the spot weld dent.
1
From Japan
On 2011-09-27 12:26:08
Freshly gratted but good, it gets clogged and it gets bad. Continued work as it is, the temperature of the base metal becomes too high and it may be distorted depending on the goods. I would like to improve the regeneration effect by examining how to plant the feathers and the base material.
This review is about item#06728093.
Deburring thin plate
5
From Japan
On 2011-05-31 20:49:07
Despite the fine grain size, the grinding amount is large and the work can proceed efficiently. I like my finish beautifully.
This review is about item#06728093.
It is used for finish polishing of metal products.
1
From Japan
On 2011-04-16 16:57:12
First of all, it is very bad that the mounting holes of baby sanders are tap of resin. There are many goods which are tapped off and there are also goods which have firm resin and can be used but this product is weak in nature of resin and sticks to the thread mount with heat with vibration and load and heat due to rotation I could not take it. I tried using one and it became such a symptom. I made it by making a tap part big and making it a foolish hole but it did not go well.
This review is about item#06728093.
Cast polishing of aluminum castings
5
From Japan
On 2010-11-12 14:59:49
Sometimes it is difficult for screws to come in.
This review is about item#07320616.
Purchased as rough skin treatment of foundry aluminum
3
From Japan
On 2010-11-04 08:35:10
I thought that it was # 80 for the rough treatment, but it seems that it was a bit sweet, so I learned that the grain size was too rough even for rough cutting.
This review is about item#06728093.
Rough cutting of wood
4
From Japan
On 2010-09-25 18:42:19
I would like to raise the adhesion strength of the abrasive.
This review is about item#07320616.
1