Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of B Type Clamp

B Type Clamp
Sales Price: -
Review Rating: 3.73
37 Customer Reviews
5 star 16
4 star 5
3 star 10
2 star 2
1 star 4
The reviews are automatic translation.
Showing 1 - 20 of 37 Reviews
Machining
3
From Japan
On 2017-03-24 18:33:48
There is no problem. In addition, I will purchase it if necessary.
This review is about item#6731173.
welding
4
From Japan
On 2015-11-24 09:42:54
I feel that cost performance is excellent
This review is about item#06731182.
For fittings
5
From Japan
On 2015-05-07 19:15:53
Cost performance is the best. There is no problem with use, it is GOOD.
This review is about item#06731182.
To fix parts
5
From Japan
On 2014-12-13 16:08:03
This quality is very good at this price. Discontinuation of handling as far as stock is disappointing.
This review is about item#06731182.
Pull out the ball joint
5
From Japan
On 2014-10-23 15:03:09
It is good to buy at this price! There is strength as well. It might be better if there is rigidity of the handle screw part. Cost performance is high.
This review is about item#06731182.
Maintenance of material members during steel welding
4
From Japan
On 2014-02-28 17:48:48
Although the comfort was relatively good, in the future it will be a clamp for plating as it will not move if sparks fly to the threaded part. This clamp is used for fixing the wood at the time of bonding.
This review is about item#06731182.
As a clamp at the time of welding
3
From Japan
On 2014-02-05 13:23:10
There is no problem in use feeling.
This review is about item#06731182.
Large woodwork temporary fixation
5
From Japan
On 2014-02-02 17:50:01
I am very satisfied that the frontage is firmly tightened and tightened with a large frontage. Cost performance is outstanding especially for the price.
This review is about item#06731182.
When fixing objects to pillars, when nails can not be used.
5
From Japan
On 2013-09-22 23:37:16
When fixing to the pillar, the pillar and the fixed object are likely to be scratched, and the thin plywood board is put in between and used. The thin plywood board protruded from the contact part of the clamp, and it appeared somewhat ugly. (It would be nice to work thin veneer boards to match the shape of the clamp over time, but stopped because it took time and effort to stop.) Felt that is easy to remove, even felt that matches the shape of the clamp is also included if convenient I thought.
This review is about item#06731182.
Fixed
2
From Japan
On 2013-07-26 18:06:34
Fixing an object of 200 mm with this clamp requires space of 400 mm. Since only large objects are fixed, if the screw is about 50 mm, it is user-friendly.
This review is about item#06731191.
Bead dropping when moped tire is exchanged
5
From Japan
On 2013-07-10 13:58:24
It was lighter and cheaper than I thought, but I'm sorry that Sara's hit part at the tip of the screw is oblique, I want you to devise a method that this Sarah part does not turn with the screw.
This review is about item#06731182.
Holding iron plate
1
From Japan
On 2013-07-05 16:30:13
It is not usable, because the angle of oscillation of the holding part of the tip is too small and the engagement between the receiving side of the tip and the shape of the end of the shaft is bad, if you tighten it, scratches will be made around the iron plate around the receiving end, the thing of the thing of the house center in the neighborhood It's better (made in Taiwan)
This review is about item#06731182.
Holding on working
5
From Japan
On 2013-04-01 20:23:36
It can be used normally
This review is about item#06731155.
Use it when squeezing members when welding.
5
From Japan
On 2013-03-23 09:38:14
Cheaply, the clamps are in good condition. Recommended, good for cheap
This review is about item#06731155.
For fixing
3
From Japan
On 2013-02-15 10:08:58
Everything is normal. I am dissatisfied with how to raise the price
This review is about item#06731137.
Temporary fixation of outdoor structures and clamps until bonds solidify
3
From Japan
On 2013-01-11 16:31:14
Unfortunately it can not be used for unacceptable failure at the work site because it is suitable for the price. Since it is not made like that in the first place, that part is evenly divisible. I think Monotaro is just a bit cheap to buy at once.
This review is about item#06731164.
Support for improvement work etc., when using tools
5
From Japan
On 2012-12-25 07:51:20
Both price and tolerance are affordable and assist with various scenes.
This review is about item#06731155.
Fastening during welding
3
From Japan
On 2012-12-24 21:03:25
Price is reasonable item,
This review is about item#06731173.
Used as a trailer platform for spring work
5
From Japan
On 2012-09-25 11:40:35
Effective width is exactly cheap, cost vs expensive and satisfactory. The body is also smooth feeling and good touch.
This review is about item#06731164.
Temporary fixation etc. at the time of welding fixed assembly etc.
4
From Japan
On 2012-07-22 01:36:21
Stable fixing by the robustness of making, so easy to use
This review is about item#06731155.
1 2
Customer Who Viewed This Item Also Viewed
F Clamps
Press C clamp
C-Clamp,  Bahco Type
Wide clamp
B Type Clamp
Bako Type C-Clamp
C Type Screw Clamps
Strong B Type Clamp
Steel C-Clamps
Aluminum C-Clamps
Joint for plastic chain
C-clamp (bar code type)
With soft grip pliers