Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Vise pliers, for welding

Vise pliers, for welding
Sales Price: 25.99 SGD
Review Rating: 4.11
9 Customer Reviews
5 star 6
4 star 0
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
When repairing the frame of the motorcycle
3
From Japan
On 2017-09-06 15:23:52
The price is attractive, but the accuracy is sweet, the mouth is distorted and closed. I caulked the rivet with a press and became a little somewhat, but I feel the construction is rough. There is no problem with the function of pinching and fixing, but a little sorry.
This review is about item#35308271.
Vice pliers
5
From Japan
On 2016-11-03 22:59:18
For exchanging tires, it is just right to use. Purchase.
This review is about item#6731365.
Fixed
5
From Japan
On 2016-04-21 17:55:42
Unlike photographs, release part is different from photograph, unlocking method is opposite to conventional product, so it may be difficult to use for unfamiliar person. I like this method so I am very satisfied. In the case of conventional products, when they are out of control at the time of releasing, the handle is hitting the finger with reaction against release, and it may be very painful.
This review is about item#35308271.
Fastening when welding automobile panel
5
From Japan
On 2014-07-27 13:36:45
The rattling, the chill of the holding part is not good. I think that it is unsuitable for precise welding, but it is not a problem to use as automobile sheet metal paint. With this product, it is good to have around the center pillar and side sill, there is a shape that can be used with the door attached.
This review is about item#35308271.
Welding operation
3
From Japan
On 2013-06-19 09:25:32
When a beginner butt welded two flat wires, I purchased it thinking that it should not be misaligned. The feeling of use is generally good, but one of the two purchased was that the left and right chin angles were not the same and the flat bar was displaced when pinched. Although we fixed it, it is appreciated if you can consider more about individual quality.
This review is about item#35308271.
Welding etc.
5
From Japan
On 2013-05-04 07:34:21
It is convenient to weld between jaws. Because of the width of the jaw, it is also widely used as a clamp.
This review is about item#35308271.
For fixing weldment
5
From Japan
On 2013-02-21 13:13:28
Although I have not used it yet, I think that it is good to look at the whole.
This review is about item#35308271.
For fixation during welding and brazing of thin iron plates etc.
1
From Japan
On 2012-11-01 19:16:32
The making itself seems to be strong, but the interval of the mouth when closed was right and left irregular and it did not match with Pitta at all. Because it is troublesome to return, we corrected the root of the jagger who is crazy by red hot in the banner. Since the application is fixed in superimposition of thin plates, there seems to be no thing that the thickness of the plate itself is thick and it will not be usable as it is burnt. I'd like you to inspect finished goods at the manufacturing stage.
Fixation of processed articles
5
From Japan
On 2010-04-06 11:38:38
There is no madness of the finish, strength and ease of use have no problem. I am happy to buy it cheaply.
This review is about item#06731365.
1
Customer Who Viewed This Item Also Viewed
Pad Lock Clamp
Vise pliers
Locking C Clamp
C type locking pliers
Vise pliers, C type
C type locking pliers
LOCKING PLIERS
Shrimp Vice Pliers
Sheet Metal Clamp
Welding Clamp
Vice Pliers C Type
Shrimp Vice Pliers
Replacement blade Mozart 2884