Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Arm crimp plier

Arm crimp plier
Sales Price: 119.99 SGD
Review Rating: 4.50
8 Customer Reviews
5 star 5
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Production of clutch wire for agricultural machinery
5
From Japan
On 2018-04-07 20:21:33
I bought without hesitating because I borrowed things from acquaintances before, so user friendliness was good. I think that individual differences do not come out as caulking is perfect as grasping the lever. If the frequency of use is high, it is one recommended item.
This review is about item#2188584.
Used for wire processing to hang a signboard of a store
4
From Japan
On 2017-09-26 23:37:43
I was surprised because it was bigger than I imagined, but I am satisfied with the work I expected. I had the opportunity to lift it to a position higher than my head and use it a bit hard to tighten.
This review is about item#2188584.
Wire construction
4
From Japan
On 2017-05-06 16:57:26
It is rather tight to close 3 mm wire. It's up to 3.5 mm, but it's easier to use the one above.
This review is about item#2188584.
Used for caulking thin wire
3
From Japan
On 2016-03-30 19:33:12
The price is too high, even if there are not so many times of use it is used because there is a crimping on your own
This review is about item#02188593.
Wire sling creation
5
From Japan
On 2015-10-14 22:15:39
It was very easy to crimp the aluminum sleeve, it was a finish that I could consent without the power I thought needed.
This review is about item#02188593.
Cutting, crimping of wire -
5
From Japan
On 2015-10-14 15:28:24
With this size, you can easily cut and caulk, the price is also cheap and satisfactory.
This review is about item#02188593.
Cut by wire
5
From Japan
On 2015-01-23 10:31:57
It is very easy to use because it has a good finish, but I also have large size items, but most of the work is using this
This review is about item#02188584.
Winch wire exchange
5
From Japan
On 2013-05-23 13:07:35
I am very satisfied with easy use.
This review is about item#02188584.
1
Customer Who Viewed This Item Also Viewed
Wire Rope Sleeve
Arm Oval Sleeve, Aluminum
Aluminum Sleeve
Aluminum Clamp Pipe
Clamp Cutter
Circular Sleeve
Oval Sleeve
Wire Clamp Plier
Strong Type Crimping Tool
Wire Clamp Plier
Arms ager 1000mm
Asahi iron jingis hotpot
Arms engager