Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Board Anchor

Board Anchor
Sales Price: 35.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
As a gypsum board anchor for home appliances, lighting equipment, air conditioning construction etc.
5
From Japan
On 2017-11-25 22:48:53
As a gypsum board anchor, a simplified type is also used, but this can be used for ceiling because it can be securely fixed, but it will not loosen although it takes time and effort to install. However, it is easy to lose the fixing pins when fixing the anchor, so I want to be careful.
This review is about item#2273826.
Work
5
From Japan
On 2015-10-21 14:50:56
Very well for the price, I would like to continue using it in the future.
This review is about item#02273783.
Other installation work including air conditioner installation work
5
From Japan
On 2012-07-24 12:13:23
The goods themselves are not problematic, but the delivery of the monotail is problematic. When I requested more than one, I came with other goods, but the contents of the board anchor were lit and the contents were scattered. I planned to give it to each person in charge for each pack, but it was serious that I had to count the number because contents were scattered. Since it is supposed to be 1 packing with 6 pieces, I think that it is in a box in 6 units or it is troublesome but I think that it is quite different simply by holding the lid about 2 places with cellophane tape etc. . Moreover, since the outer box of the packaging is a cardboard of Yorereye, depending on the situation, I think that board anchor that jumped out of the case has gone out of the gaps and holes of the box. Moreover, it will not be possible to deny the possibility that it will be crushed and not used as it comes out from the case, so I want you to use a little more care in packing.
This review is about item#02273835.
Air conditioner indoor unit installation and others
5
From Japan
On 2012-06-17 20:45:22
It is still easy to install, there is strength
This review is about item#02273835.
It was used when installing control board etc to gypsum board.
1
From Japan
On 2011-11-08 16:53:40
I made a specified hole in the gypsum board and turned this product with an embedded hook, but the protruding part stuck on the board surface of the main body dug a large hole in the board as the role of the drill. I thought that how to use it was bad, I put it in the embedded state and turned the holding hook with a pliers, but the part with the protrusion breaks in a few times very hardly and the anchor can not be removed It was. As an improvement point, I think whether it can be supported by protrusions as the body breaks more softly.
This review is about item#02273792.
1
Customer Who Viewed This Item Also Viewed
Wall Anchor, Pack Product
Board Anchor
Board Anchor
Board Fastener 10pcs
Board Anchor
Toggler
Drywall Anchor
Wall Anchor
Easy Time Board Anchor
Board Anchor Tool
Protech, Board Anchor
Board Fastener 8pcs
Sleeve Anchor
Cavity Wall Anchor
Board Fastener 12pcs
Board Anchor