Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of FA HOLE CUTTER (WITH SUPER HARD CARBIDE TIPS)

FA HOLE CUTTER (WITH SUPER HARD CARBIDE TIPS)
Sales Price: 47.99 SGD
Review Rating: 3.00
4 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Drill a hole in a single pipe
1
From Japan
On 2015-05-15 19:07:57
I received it today as soon as it arrived. I opened two holes in a single pipe, I got one tip I managed to open a hole somehow, but I was disappointed that it was a bad method or a defective item.
This review is about item#03396355.
Drilling of steel material
5
From Japan
On 2015-03-17 19:33:18
I have opened Φ 20 already in 50 holes or more in steel material drilling (t 6 mm), but there is no problem at all. It is the first purchase with DIY. A commercially available drilling machine, cutting oil is cheap oil spray of Homusen. But one to four will be lost with 4 to 5 holes .... I bought two, but it may be good with one. I think that it is recommended privately.
This review is about item#05609143.
Casting processing and other die-casting processing
5
From Japan
On 2010-10-12 22:59:35
Cutting edge is being scrutinized Sharpness is sustained and accurate point work is done It can do a good work as price does.
This review is about item#05609186.
I attached it to a hand borer and drilled in a round pipe about 3 mm in thickness.
1
From Japan
On 2010-08-09 18:34:57
In half a day super-steel chips flew 3 points out of 4 points and disappeared. Are they comparing durability with other companies' products?
This review is about item#03396346.
1