Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Bearing Washer

Bearing Washer
Sales Price: 0.99 SGD
Review Rating: 4.14
7 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
As it is a part, it is not used for work. "
From Japan
On 2017-12-24 06:43:04
I occasionally use it, but it was as planned as usual.
This review is about item#05823456.
During machine repair
From Japan
On 2017-06-10 16:35:54
Shipments are also very satisfied quickly with solid products.
This review is about item#5823517.
Used when replacing machine parts
From Japan
On 2016-11-12 07:07:50
It is purchase with repeat. The price is also cheap, the quality itself is not problematic, though. However, among the items I bought this time, there was one screw bent so badly that I had a hard time installing it. It is a bit disappointing. So, although it is originally four stars, this time it is two stars.
This review is about item#05823501.
Used when replacing bearing bearings
From Japan
On 2016-08-12 05:34:33
Especially it was able to be used without problems. Compared to what was used from the beginning, I felt that the claws were hard, but there is no problem at all.
This review is about item#05823501.
From Japan
On 2016-02-22 23:16:20
Very good, finished.
This review is about item#05823535.
Used as tapered metal for tapered roller bearings
From Japan
On 2015-10-16 14:55:51
Since the bearings of the board (daughter) which carries the motorcycle move is rattled when the ground is rattled, it is impossible for usual things to happen, so we built and modified tapered roller bearing bearings. At that time, I was looking for a circular one that pressed the moving part of the bearing against the plate, but I found this product and tried it. The tapered roller bearing bearings were at hand, and the size was perfect as we chose the item while measuring its diameter. If you tighten with bolts, the peripheral fold spreading in the Z axis direction will collapse, but it will be strong enough to hit the board and it will be enough slip prevention. I wonder if the inside protuberance of the circle did not enter me? I cut it with a ruther and used it.
This review is about item#05823465.
Repair of concrete mixer bearings
From Japan
On 2015-02-09 19:10:41
I was looking for them. It was nice to have parts. It is Monotaro-sama! It is!
This review is about item#05823544.
Customer Who Viewed This Item Also Viewed
Nuts for Rolling Bearings
Self-Locking Nut
Lock nut for bearing
Bearing Nut
Bearing washer
Chain for lock pin
Washer (stainless steel)
Adapter Nut
Power lock EF series
NRPF series
Washer for rolling bearing