Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Eyebolt, M Screw

Eyebolt, M Screw
Sales Price: 2.99 SGD
Review Rating: 2.44
9 Customer Reviews
5 star 2
4 star 0
3 star 2
2 star 1
1 star 4
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
As eyebolt and
3
From Japan
On 2017-03-24 16:45:23
There is no problem as an eyebolt. We will also purchase
This review is about item#6563611.
Yamaha motorcycle cylinder bed when disassembled
1
From Japan
On 2016-12-27 07:25:25
I used it to hang a sliding hammer off Majesty's rocker arm shaft but I want a little more strength
This review is about item#6563602.
Lifting work of heavy objects
5
From Japan
On 2015-08-16 18:06:00
It is necessary and sufficient function.
This review is about item#06563636.
Loading and unloading machine parts
1
From Japan
On 2013-11-27 14:59:51
Although I bought M24, it seems that the lead angle (the angle of inclination of the screw) is slightly larger compared with the original one that turns only the first few or three ridges. Is it JIS standard item? · · · There are comparative photographs arranged.
This review is about item#09427661.
Used when hanging heavy objects with a crane
1
From Japan
On 2012-12-21 14:48:23
I bought 10 items, but there were two items that I could not use. Future purchase will be considered if 20% can not be used. Please check the usability and test whether it can withstand the weight. I think that not checking whether it can be used is not done other tests. Thanking you in advance.
This review is about item#06789937.
Lifting up of casting parts etc.
5
From Japan
On 2012-11-23 11:04:18
I purchased 10 M16s. I saw a review that sometimes it is necessary to screw it back, but none of the things I bought this time was problematic. I will purchase again when necessary.
This review is about item#06563636.
It is planned to be used for lifting a heavy object of 0.5 t.
2
From Japan
On 2012-02-15 10:47:35
Since I heard that you need to re-screw with the comment information beforehand, it took time to deliver the product after it arrived, so once you have passed through the dice, there are things that scrape off the valley of the screw as "hair" There were also things of repair. (Shuffle around the mountain) The eyebolt has taken an X mark as "NG item" because it takes time to correct. The price is cheaper than other companies, but if it seems there are more nonconforming items than it is now, you may not buy it in the future. Three of the four were able to fix with a die thread, one was NG.
This review is about item#06789937.
...
1
From Japan
On 2011-12-03 13:30:23
I had to screw it with a dice and the nut did not turn. It's the worst.
This review is about item#06563627.
Attach suspension wire of measuring machine
3
From Japan
On 2008-12-01 08:36:43
no problem
This review is about item#06563627.
1
Customer Who Viewed This Item Also Viewed
Eye Bolt
Long Eye Bolt, Metric Thread
Long Eye Bolt
Eyebolt, Milli Screw
Eyebolt, W Screw
Eye Bolt, Iron Chromate
Uni Chromate Plated Eye Bolt
Eyebolt
Eye Bolt
Eyebolt
Eyebolt (iron / Dov)
WATERPROOF HINGES
Steel Eye Bolts
Eyebolt