Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Clean Paperboard

Clean Paperboard
Sales Price: 22.99 SGD
Review Rating: 4.33
6 Customer Reviews
5 star 4
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
It is used for work such as automobile repair.
3
From Japan
On 2016-01-13 17:19:09
It is saved because it does not have to be cleaned after use because it is disposable. However, as you use it in half, the board and paper are peeled off at any time, I use it with tape, but it is very good, but I will do my best to improve the neighborhood, but thank you.
This review is about item#05490441.
As a platen of the vehicle sheet metal
5
From Japan
On 2015-02-19 21:57:25
Weight, hardness, quality of paper, ease of handling is perfect. I ordered an additional order. I was looking for Kore!
This review is about item#05490441.
Two-wheeled, four-wheeled sheet metal
5
From Japan
On 2014-11-23 14:15:53
It saved my labor for cleaning and it became very easy. I definitely would like to purchase as well!
sheet metal
5
From Japan
On 2014-09-05 19:16:24
I think that it is convenient and good product. Just turn it over. It's easy. It is made of coated paper, so it gets wet and the surface seems to be waving after drying. But you can use it. It is cheaper than a real store, but there seems to be some cheaper places in mail order.
This review is about item#05490441.
Automobile sheet metal · painting work
3
From Japan
On 2013-01-18 12:22:43
Sheet metal of automobile · It is used for putting work during painting work. It is the same as the purchase of a paint shop dealer, but since it is a high use frequency we would like to ask for further price reduction. Is it a bit cheaper compared to a paint shop in terms of price?
This review is about item#05490441.
As a putty of putty
5
From Japan
On 2009-06-16 12:44:53
Since it is laborious to clean it with an aluminum platen, disposable paper boards are useful.
1
Customer Who Viewed This Item Also Viewed
Plastic Cladding Plate
Putty Plate
Putty Cladding Plate With Stainless Steel
Solder Aid
Star bit with socket (T15)
Putty surface plate
Outty Peak Board M-Shape
Stainless Putty Board
Stainless Putty Board
Tubular tablet display tablet
Zoom type Stereomicroscope NSW-40ILM-260
Putty surface plate
Miniature ball valve