Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Set Terminal Block T30

Set Terminal Block T30
Sales Price: 6.99 SGD
Review Rating: 3.60
5 Customer Reviews
5 star 2
4 star 0
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Vehicle wiring
5
From Japan
On 2017-11-11 18:22:43
I always use it. I think that there is no problem. I will continue to use it.
This review is about item#6945793.
Distribution board from generator on site
3
From Japan
On 2015-02-28 18:17:03
Easy to use
This review is about item#06945784.
Relay wiring between the testing machine and the device under test
3
From Japan
On 2014-11-19 10:16:34
For wiring, use a cord with a crimp round terminal normally. I screw it, but as you move the cord, the screw loosens and it moves soon and it seems to come off. Although it is a structure to suppress the screw with a mountain of crosses when seeing it, since the contact area is small, the power of holding down is insufficient. So I use all the screws instead of ordinary sems screws, flat washers, spring washers. Also, since it is an iron screw, the electric resistance is large, and if you want to say it, the resistance loss should be reduced by the brass screw.
This review is about item#06945793.
Independent solar power generation
5
From Japan
On 2014-04-21 08:17:56
Truly Kasuga Electric, a sense of security when crimping terminals are tightened! It is! Best
This review is about item#06945802.
For wire connection terminal branch
2
From Japan
On 2014-01-10 12:13:27
The screw part is weak, and when it is fitted or removed many times, the screw will become difficult to tighten. I feel that the strength of the screw part is weak.
This review is about item#06945793.
1
Customer Who Viewed This Item Also Viewed
Set Terminal Block T100
Group Terminal Block T20
Set Terminal Block T10
Set Terminal Block T200
Set Terminal Block T60
Jumper Metal Fitting
Fork Terminal Stripes
Terminal Block Accessories
Group Terminal Block
Short Bar B-Type
CUNO Micro-Screen
Combined terminal block