Customer Reviews of Set Terminal Block T60
|
|
---|
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Terminal connection

From Japan
On 2017-02-11 09:37:13
I think that it is a good product. I could easily connect the terminals. It is a necessity for electric construction.
This review is about item#6945915.
Parts in the control panel

From Japan
On 2016-12-21 14:50:41
Thank you for the black mark you would like me to write what amperes withstand pressure in the product's bevel. For misuse prevention
This review is about item#6945881.
DC power distribution

From Japan
On 2015-03-22 19:20:22
I chose a bit oversized so I am very satisfied with satisfaction.
This review is about item#06945906.
It is used for wiring of in-house power generation equipment.

From Japan
On 2013-10-20 15:00:05
I bought it as a terminal block of TC - 60 terminal stand independent type solar power generation by Kasuga Denki. Because it can flow up to 50 A at the low voltage, it thought that it did not generate heat. The thickness of the conductive plate is about 2.6 mm and it is quite thick and there is a sense of security. Originally it should be able to pass more, somewhat excessive grade? Crimp terminals can be used with M5 to M6 specifications with a width of 12.5 mm. If it is a single core electric wire such as VVF, it can be wrapped and tightened. T-30 of the same manufacturer with cheap price was also a candidate, but if it goes up to 30 A it wants to recommend TC - 60 if it exceeds T - 30, 50 A.
This review is about item#06945897.
1