Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Standard Set Color SUS304

Standard Set Color SUS304
Sales Price: 2.99 SGD
Review Rating: 3.80
10 Customer Reviews
5 star 6
4 star 0
3 star 2
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Creating rotating equipment shaft
5
From Japan
On 2017-08-02 14:34:20
It is a thing that is not sold to the home center, so it is appreciated. Bore size / external shape can also be selected. I am satisfied with high precision.
This review is about item#06941742.
Stopper of the stand of the camera stand
3
From Japan
On 2017-01-09 10:35:52
It is most stable and preferable that there are two set screws at the 120 ° position, but there are many small scratches on the product, and the looks are not good.
This review is about item#6941715.
Fastening of parts of precision equipment
5
From Japan
On 2016-11-29 17:59:18
I have reassured that it is a Japanese product, as expected though there is goodness of fit as if it was manufactured according to the parts here. Packaging was polite and it was saved as soon as I arrived. Thank you very much.
This review is about item#6941654.
As a DIY
3
From Japan
On 2016-08-08 20:37:06
I have never compared it with others, so I guess like this.
This review is about item#6941444.
Tone arm sub weight
5
From Japan
On 2015-09-14 15:52:06
As a subway of the tone arm of the record player, similar products are sold at the 2,000 yen level, but this is equal and it is very profitable with the beauty of material, accuracy and finish. Because it is a product with a diameter of 14 mm plus plus error slightly, caliper precisely stops at 14 mm diameter arm precisely. Although it thinks that there are many persons for orthophone SPU attachment purpose in this use, it balances well also in terms of weight and there is no obstacle such as chattering sound because it is stopped by screws. There is no discomfort because the appearance is also a color tone that is similar to ordinary balance weight.
This review is about item#06941541.
Analog Player Sub Wait
5
From Japan
On 2014-06-05 13:27:19
With good finish of goods, even if you attach it to the player's arm it does not feel uncomfortable. Screw fixation was able to be tightened with regulation which does not hurt the existing pipe. It was a very accurate and excellent product. I would like to purchase it for another player.
This review is about item#06941697.
I tried to use it as a flywheel for 13000 rpm cutting router
1
From Japan
On 2013-09-12 00:39:27
The cutting system is very nice, it fits perfectly on the 10 φ spindle, and it could be tightened without rattling of the set screw. Distortion due to excessive tightening is also not recognized. Due to the shape, dynamic balance was not taken at all, core shake occurred, and performance as expected could not be demonstrated. The function as a shaft stop in the thrust direction has no problem at all. It is a great help if you specify clearly the maximum allowable speed. I want a set color with dynamic balance guaranteed.
This review is about item#06941444.
Supplementary weight of record player's arm
5
From Japan
On 2013-09-11 08:37:14
I bought a player called GT - 2000 of YMAHA and bought the cartridge of SPU of Ortofon this time, because the weight of its cartridge is heavy, I bought these three types of same color set as an auxiliary weight. Those close to genuine for audio are quite expensive, but we are very satisfied with the highest precision as general purpose.
This review is about item#06941654.
Securing the shaft
5
From Japan
On 2013-03-08 18:18:08
Since it is a used product, it can be used without problems.
This review is about item#06941444.
Securing the shaft
1
From Japan
On 2012-01-01 17:52:57
In the item description, one set screw was attached, so in the drawing it was two screw holes, so at the same time I bought a hexagon socket head fastening screw and thought about tightening at 2 places, but there was only one screw hole. It can not be tightened in two places. Although the attached screw is SUS M3 (should be), the hexagon socket is not tightened with cabbage. At the same time I bought M3 Hexagon socket screw Kubomi (stainless steel) Osaka soul is also quite cute but it is more severe than that. Since hex wrench can not be used Bondas, we tightened with 1/16 inch hex wrench. It is an explanation that the chamfer is 45 degrees on one side and 30 degrees on one side, but it can not be distinguished by appearance.
This review is about item#06941313.
1
Customer Who Viewed This Item Also Viewed
Shaft Collar Standard Type
Set Collar Standard Type
Stainless Steel Shaft Collar Standard Type
Standard Set Collar
Set Collar
Set color stainless steel SUS
Standard set color
Standard slit collar SUS 304
Stainless steel set color