Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Seven Lob Knob Stainless Steel External Thread

Seven Lob Knob Stainless Steel External Thread
Sales Price: 4.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Used for furniture parts adjustment section
5
From Japan
On 2017-06-06 07:25:27
Since the finished state was good, it blended fully into furniture under use, and the image was good.
This review is about item#07003631.
Used for maintenance of agricultural machinery
4
From Japan
On 2016-11-04 19:18:21
Even if it is a genuine product, when a load is applied to the thread, the screw part material is bad and it has been loosened by vibration, so we were looking for good material but there was what I was looking for So I bought it. The feeling of use seems to be the feeling that agricultural machinery has been using for a period of use (until next autumn use).
This review is about item#7003762.
As a stopper to expand and contract the pipe
5
From Japan
On 2016-11-02 18:16:05
Because it is a small diameter screw, the grip is small, but the force is transmitted properly,
This review is about item#7003665.
Tightening the screw
5
From Japan
On 2016-03-24 20:03:50
It was saved for screw tightening in a place where tools are not needed or where tools can not be used.
This review is about item#07003631.
For hobby's work in DIY
5
From Japan
On 2013-02-14 18:27:42
Grip was easy to grasp as the singing phrase, I felt that it was more familiar to hands than other triangles and crosses and easy to handle with other products. Although the screw part is particularly unavailable and impossible, "● Material (threaded part): SUM22L ● Surface treatment (screw part): UNIQLO plating" is shown in the description of the product which is "made of stainless steel". I think that it is a mistake of SUS 303, but I got lost a little.
This review is about item#07003692.
1
Customer Who Viewed This Item Also Viewed
Seven Lob Knob, - External Thread Made From Steel-- M5
Grill Knobs
Plastic Cross-Joint Knob
Plastic Lobe Knob
Taped blind knob BTK-L-sus
Lobe Knob Nut
Lobe Knob Bolt
Small knob stainless steel (male thread) SK-sus
Seven Lobed Knob M12, Steel, Male Screw
Grill Knobs