Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Fuse-Holder Junction Type

Fuse-Holder Junction Type
Sales Price: 0.71 SGD
Review Rating: 3.90
10 Customer Reviews
5 star 3
4 star 4
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
For bike wiring
4
From Japan
On 2017-10-26 23:52:00
Although it may be a simple structure, is not it possible to make it more compact if we review the shape a bit more? (Especially length) I think that it is a little untitled big.
This review is about item#6953527.
Wiring of weak electric devices
5
From Japan
On 2017-08-16 16:01:05
Used to put a fuse in the relay section of the wire. I imagined a bit bigger, but I think it is very good as it takes less space.
This review is about item#6953606.
When installing car accessories
4
From Japan
On 2017-04-30 19:35:10
It is inexpensive, but it is firm making. Although this time it is used inside the car, there is no problem, but it may be tough to use in places with excessive vibration such as engine room.
This review is about item#6953606.
Used for protection of wiring for power supply.
3
From Japan
On 2016-10-06 11:12:41
The F-22 is easy to solder the electrode terminal, but it is a disadvantage that it is difficult for the holder to open when replacing the fuse. The F - 7160 is a terminal that is hard to solder with the opposite direction, but replacement of the fuse is easy because it is a screw type.
This review is about item#08621943.
Protection of electrical components
4
From Japan
On 2016-06-10 16:53:31
Although other people review that the springs will fly when replacing the fuse, I think that it is an error in the installation method. There is no flying if soldering the washer through the wiring through the spring. I need some tips for soldering, but I agree with this price.
This review is about item#06953606.
Addition of fuse to unstable electric products
2
From Japan
On 2015-10-21 11:31:27
It was so cheap that I jumped, but the springs that must solder the internal parts (springs, terminals etc.) inside the holder and solder their own wires will move freely, so if you fuse you lost somewhere and lose something Possibility large. Well, I wish I could put more price
This review is about item#06953606.
Protection of test wire
4
From Japan
On 2015-10-10 18:46:28
I bought it because the electrical standard was the best in the series. It is said that contact failure will occur if the electric wire is pulled from the structure. I think that it is used for other types if it is less than 3A.
This review is about item#06953527.
Electric fence
3
From Japan
On 2015-09-25 22:47:12
A washer connecting a cable is a chat.
This review is about item#06953606.
Car wiring
5
From Japan
On 2015-05-17 16:20:11
It is durable and easy to use. I think that it is better not to stand out from the white type.
This review is about item#06953527.
Prototype of electric circuit
5
From Japan
On 2014-11-13 13:34:14
Especially it was able to be used without problems.
This review is about item#06953527.
1
Customer Who Viewed This Item Also Viewed
Pipe Fuse
B Type Fusing Type Fuse Fgb0
Fuse Holder F-800
High Fault Relay
Fuse-Holder
Relay Fuse Holder MF-520
Fuse-Holder Junction Type
Pipe Fuse-Holder
Fuse Holder, Tube Type
Pipe Fuse Holder
Pipe Fuse Holder
Glass Tube Fuse
Fuse holder relay
Fuse-Holder
Fuse Holder