Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Single-Row Deep Groove Ball Bearing No. 6900 Stand Vv, Both-Sides Non-Contact Rubber Seal Type

Single-Row Deep Groove Ball Bearing No. 6900 Stand Vv, Both-Sides Non-Contact Rubber Seal Type
5 star 4
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
I used it for a sprocket of a motorcycle.
5
From Japan
On 2017-08-10 18:42:51
Smooth motion is required as it is used for gear change parts. It is thin and compact, but it plays a full role.
This review is about item#6955286.
For changing the hub bearing of the bicycle
5
From Japan
On 2016-07-19 17:06:43
The place where I bought a used wheel whose mileage is unknown, since the bearing of the metal shield was included in the hub which should normally have the ordinary rubber shield bearing, it was playfully exchanged and exchanged with this product. NSK of fluffy, it was cheap but it was perfectly accurate. When I tried opening the seal, a transparent amount of grease was sealed in an appropriate amount. The feeling turned by hand is smooth. Since the rear side can not usually do much work, change it while staying normal. The front side sealed extremely pressure grease after completely degreasing. Although slightly turns lightly, since it hardly changes, it is not recommended to forcibly replace grease. It is too much performance for commuting wheels.
This review is about item#06955295.
Motorcycle engine
5
From Japan
On 2016-07-07 09:46:05
From now on purchase from genuine products and quit.
This review is about item#06955313.
Maintenance parts for original mind CNC milling machine
3
From Japan
On 2016-02-09 07:05:01
I purchased it as a spare for the replacement of the bearings used in the spindle unit. Manufacturers may be different, but standards are the same, so it should be used without problems. For those who frequently use CNC milling machines, it is a recommended item. The higher the rotation speed, the more the bearing balls will be worn out, so that the rotation shaft may be blurred, making it impossible to perform beautiful machining, opening a hole larger than the specified size, or causing distorted holes to open. If you think that machining accuracy has deteriorated, it is better to replace it earlier. We recommend that you use a bearing pooler when removing the bearing with bearing exchange. (I made a special puller at a low price, but since it can only use the original mind CNC milling machine, it may be better to sell it on the market.)
This review is about item#06955277.
As a vehicle wheel bearing.
5
From Japan
On 2014-03-11 13:49:47
Although I have not used it yet, I am safe because it is an NSK product.
This review is about item#06955322.
1
Customer Who Viewed This Item Also Viewed
Blind rivet all steel