Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Analog Multitester

Analog Multitester
Sales Price: 61.99 SGD
Review Rating: 4.20
5 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
General work
1
From Japan
On 2018-01-14 00:55:20
I arrived yesterday and used today, it will not stabilize AC range can not be used at the beginning, the resistance range has become strange and it has stabilized when I used it several times The same symptoms first at the time of the previous purchase also result, it is not stable to the end Discarded at Although the instruments were purchased at a specialty shop, I tried using it conveniently There was no similar posting, the Sanwa electric instruments tester was necessarily required for our work, but it was easy to break into the case, but this time it was a brand new unopened state so it was a last time It is not a complaint that I also posted on things, but I think that if you have similar posts you should check with Sanwa-san
This review is about item#3358677.
Used for inspection of electrical fuse and ignition circuit (mainly resistance measurement)
5
From Japan
On 2017-07-06 11:08:21
If it is digital (because of sampling) the value may not be stable, purchased as a sub machine for its compensation. In the case of a small analog tester, the representation of the range of 10 Ω or less (the comma or less is unnecessary) of the range is small (narrow) in many cases, and there was not any suitable thing in the case of a small analog tester However, this model is easy to use because the corresponding range width is widely written comparatively. Since fixing of the probe is original method, there is a problem in the case of disconnection etc. However, because the probe for repair is also sold at a low price inexpensively, it is recommended to purchase the spare of probes as well. There are two positions where the number of poles of the rotary switch is over or OFF, but ... If the two places are not two next to each other, the design of the user interface that positions it at 12 o'clock and 6 o'clock is kind Then, this is only a question.
This review is about item#3358677.
work
5
From Japan
On 2017-04-28 22:00:39
It is small and easy to use Because the performance is also good, I am saved
This review is about item#3358677.
Maintenance of communication equipment
5
From Japan
On 2016-11-16 15:28:58
I used it before but broke the previous one and purchased the same again. Very easy to use.
This review is about item#3358677.
Electric installation inspection check
5
From Japan
On 2015-03-23 16:43:30
I used the same item before, but it was easy to see, easy to use and purchased this time. The difficulty is that there are no optional items to replace as the code breaks.
This review is about item#03358677.
1
Customer Who Viewed This Item Also Viewed
Analog Multimeter
Analog Multi-Tester
Analog Multitester
Analog Multimeter, Hard Case
Analog Tester
Analog Multitester
Portable Case
Analog Multitester
Analog Multitester
Analog Multitester
[0.8mm] wire stripper
Analog Tester, Magnet
Analog Multitester
Micro Pocket-Size Analog Multi-Tester