Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Couplicon Mini Set Screw Type

Couplicon Mini Set Screw Type
Sales Price: 18.99 SGD
Review Rating: 4.62
8 Customer Reviews
5 star 6
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Power unit of radio control
5
From Japan
On 2017-10-19 09:01:32
Convenient for absorbing deviation drift of the radio control motor and drive shaft.
This review is about item#07217025.
Maintenance of radio equipment
5
From Japan
On 2017-08-01 21:23:15
Until now, I have used Steatite's universal coupling, but Cospa is also good, I am satisfied.
This review is about item#7217122.
During machine maintenance.
5
From Japan
On 2017-04-30 19:00:55
Thank you very much for reaching me as soon as possible with a good item as I expected. There is nothing to improve.
This review is about item#7217016.
Combining the motor shaft and working axis
5
From Japan
On 2017-03-28 20:35:11
Handmade machines had poor tooling accuracy and failed with flexible fittings to connect the motor shaft and the working shaft. This Oldham type fitting requires adjustment by a little bit but rotation is very light.
This review is about item#7217034.
motor
4
From Japan
On 2016-02-01 14:54:09
As I wanted, I could connect the gear with the motor. It would be even better if it is a bit cheaper,
This review is about item#07217174.
CNC
3
From Japan
On 2015-12-14 19:18:20
Lack of explanation Is it a good thing to investigate elsewhere?
This review is about item#07217393.
Connection between motor and different diameter shaft
5
From Japan
On 2015-03-29 21:09:41
Although it is still in the stage of assembly, it is also firmly attached to the shaft and rotates smoothly. Because there are many variations, it is saved.
This review is about item#07217402.
Use for school graduation research equipment manufacture
5
From Japan
On 2013-12-14 09:35:11
I tried to make a coupling by myself to join DC motors, but as the centering did not go well, I bought this product. There is neither vibration nor shake, it is in good condition. The electric motor of this time fitted with the diameter of the rotor shaft about 11 mm and had a key groove in the shaft, so it was possible to fix it well with the setscrew. The DC motor is SANYO DENKI CO. LTD DC SERVO MOTOR R 720 - 039 W 65 W 30 V 3.6 A 1050 min - 1.
This review is about item#07217506.
1
Customer Who Viewed This Item Also Viewed
Couplicon Mini Set Screw Type
SPR FLEX Coupling
Soft Flexible Coupling Couplicon MSF Series
Couplicon MRG Series
Oldham coupling
Mini Couplicon
Capricone Oldham type MOR
Capricon Oldham Type
Capricone , Mini clamping type
Capricorn Mini Clamping Type
Capricorn mini spacer
Jaw-Flex Coupling L Series
SPR FLEX Coupling
Capricone , Mini
Couplicon Mini Set Screw Type
JO MAX SS 075
Super zero Oldham coupling MMZ series
Oldham Coupling