Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Straight Shank Point Flute Tap, Tin

Straight Shank Point Flute Tap, Tin
Sales Price: 5.99 SGD
Review Rating: 4.00
7 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Tapping of metal material
5
From Japan
On 2017-05-05 17:16:38
Although it is very inexpensive, there is no problem with work. I want to repeat again
This review is about item#7227254.
When correcting the screw hole
4
From Japan
On 2016-08-08 16:48:23
It was "Lucky" at an affordable price just looking for something M3 broke just. I wonder if the quality is fine.
This review is about item#7227211.
Tap on mold material in tapping machine
5
From Japan
On 2014-12-02 16:22:36
It can be used without problems. Lifetime It is under continuous observation for the spill of the blade.
This review is about item#07227254.
Tap to 5SS 400
1
From Japan
On 2011-10-21 20:27:58
I broke up in one shot. I thought that it was some mistake, but the following also broke up in about 20 pieces of processing. I will not buy it again
Tap processing of parts
3
From Japan
On 2011-03-08 19:59:19
There are variations in the diameter of the tap (the diameter of the part tapering down from the shank). There was a thing of 3.34 mm in the tap which I bought. Since the lower diameter is 3.3 mm, there is a possibility of breaking at once if putting it deeply. It can be relieved if you make it at least between 3.0 and 3.1 mm · · ·.
This review is about item#07227227.
Part tap
5
From Japan
On 2010-11-13 12:39:51
The price is attractive and is not different from famous manufacturers
This review is about item#07227236.
Screw of M5.
5
From Japan
On 2010-10-19 18:43:13
It can be used normally. Because it is cheap, shock is small even if it breaks w
This review is about item#07227236.
1