Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Home Hoist

Home Hoist
Sales Price: 1,189.99 SGD
Review Rating: 3.00
2 Customer Reviews
5 star 1
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
Lifting work of beet seedling
1
From Japan
On 2017-04-29 16:15:51
I bought it in 2013. Since it is seedling work, it is a work once a year. Actually, we were working with lifting 50 kg of seedlings, but this year the motor ceased to move and it stopped moving. I broke the motor and the amateur and the brush part were burning. Even seedlings of 50 kg seemed to be heavy so it seems to be lacking in point. 2.5 A I think that it is impossible with a 140 W motor. I would like to investigate whether selling by motor alone.
This review is about item#7253145.
Installation of things for unloading steel materials Duct, piping installation
5
From Japan
On 2014-01-16 15:28:36
It is very light and easy to use, because the size of the main body is small such as work in a narrow ceiling or not much hanging, usability is the best! The biggest problem when using a hoist is the weight of the hoist at the time of setting the main unit, but it does not matter at all if it is this hoist. Anyway it's small and light, so it's easy to carry around. I think that it will be more convenient if the upper hook can rotate 360 ​​°.
This review is about item#07253154.
1
Customer Who Viewed This Item Also Viewed
Electric Hoists
Electric Hoists
KL-1E Swivel Hook
Chain Block
Home hoist switch
Electric Chain Hoist