Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flat Washers

Flat Washers
Sales Price: -
Review Rating: 4.57
7 Customer Reviews
5 star 5
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Clamp operation
4
From Japan
On 2013-07-22 14:02:17
I am using it without particular problem.
This review is about item#07294375.
Joint of beam and girder · Mechanical parts
5
From Japan
On 2013-04-14 08:08:54
There is no problem in using it for building / mechanical parts, but it is pleasant if it becomes a little cheaper. It is convenient to use for milling and lathe machining as parts of machines Thickness · Center of hole etc. No problem.
This review is about item#07294375.
Because it is thicker than the usual washer, it is used for adjusting the tightening margin of the nut
5
From Japan
On 2012-07-12 13:05:37
Materials Usage feeling can be used without problems. There is no particular problem in appearance.
This review is about item#07294384.
Clamping
3
From Japan
On 2012-03-15 18:35:06
Although it can be used without problems, it is regrettable that there is no 14 mm for the washer, although the bolt nut has 14 mm.
This review is about item#07294366.
For clamping workpiece
5
From Japan
On 2011-10-12 12:55:38
I could use it with difficulty.
This review is about item#07294375.
It is in use as a base for <Descending screw of spindle of desk miniature milling machine>.
5
From Japan
On 2009-06-17 02:10:38
I think that the tightening of the screw is stable since there is enough thickness.
This review is about item#07294366.
It is used to prevent the flange nut from loosening.
5
From Japan
On 2007-11-08 20:33:17
Since there was a guarantee of return, if I bought one for testing, I could use flange nuts with Naveya or even a super tool, so I lost the cheap and love it now.
This review is about item#07294366.
1
Customer Who Viewed This Item Also Viewed
High-Tension Washer, S45C / H
Flat Washers
High Tension Washer
Flat Washer
Flat Washer
Flat Washer
Flat Plain Washers
Flat washer
Flat Washer ESR
BJ743 Flat Washer
Flat Washer
Flat washer