Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Crimping Pliers, For Open Barrel Terminal / Simpl

Crimping Pliers,  For Open Barrel Terminal / Simpl
Sales Price: 56.99 SGD
Review Rating: 3.67
9 Customer Reviews
5 star 2
4 star 4
3 star 1
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Car navigation wiring Micro switch connection terminal creation
4
From Japan
On 2017-03-21 03:30:19
040 type Yazaki made female terminal crimp finish is finished neatly, but with the small flat connection terminal of (Small rocker SW) connection when the back fog line is drawn using Micro relay, the compatibility with the manufacturer can be crushed low So we used Teflon wax slippage with (tool crimp type) part improved. Although feeling of use is good at the same time, it is a point of disadvantage, although it depends on the frequency of use for the simplified type compared with others (Lobexx) etc. It is expensive.
This review is about item#07032794.
Factory encoder cable repair
2
From Japan
On 2017-03-10 18:24:15
I thought I could handle a variety of sizes, but I guess I was a bit greedy ... ... I could not successfully caulk a long honey, which was the primary objective of the very bottom. It is good to bend the tip of the honey with pliers beforehand but it is troublesome if there are many numbers. E company's pliers obtained afterwards have narrow range of correspondence, large contacts for automobiles and audio are not caulked, but it was possible to crimp (clean) neatly without pretreatment, so as a result I am using this. If you think carefully, the wiring of the car is enough for the general purpose pliers on hand, and I do not have scenes that require other sizes, so I should have chosen a product focused on the very small contact from the beginning. For those who only need a specific size like me, I think that unnecessary dice are too many and it is difficult to use.
This review is about item#7032794.
Automotive wiring processing
2
From Japan
On 2016-04-27 21:27:16
There seems to be compatibility with shapes such as crimping Giboshi and manufacturers, and there are times when it can be crimped successfully and when it makes a strange collapse.
This review is about item#07032794.
Connection of terminals
5
From Japan
On 2016-04-13 14:44:30
I have been using this product for 20 years ago but it is the best it will be another 5th line ...,,
This review is about item#07032794.
Crimp terminal
5
From Japan
On 2016-02-15 15:35:46
It was as expected.
This review is about item#07032794.
Used for crimping small connector vehicle connector
4
From Japan
On 2015-10-20 20:05:58
You can crimp securely and accurately. In the case of an open barrel with a thin plate thickness, there are cases where the tip does not curl well because there is not enough sliding in the surface of the concave mold because there is not enough slipper. If it can not be polished / chrome plated in price, it can not be helped I think that is incomplete. It is because there is no need for the same thing that does not wish to continue purchasing.
This review is about item#07032794.
Motorcycle wiring
3
From Japan
On 2015-04-24 20:03:33
Is it good if it is about half of the current high price?
This review is about item#07032794.
Used for harness creation for cars
4
From Japan
On 2013-12-05 20:03:13
I used it for making 090 type coupler. This is enough as it is not something you use everyday, but it's easy to get out if you are a bit cheaper. I am satisfied because I can firmly caulk.
This review is about item#07032794.
For terminal crimping
4
From Japan
On 2012-03-03 08:32:25
Recently there are many thin wires, so I could not crimp them with my old tools. If it is this, it is okay with a rather thin line (terminal). However, since it has no function of peeling off the wiring, it is troublesome to pick up the tool each time. It's nice to have a small one, but I do not like feeling as if I was too thin.
This review is about item#07032794.
1
Customer Who Viewed This Item Also Viewed
Crimping Tool
Precise Bonding Plier
Open Barrel Type Contact Crimping Tool
Chain Type Crimp Terminal Crimping Tool
Crimping Pliers
Crimping Pliers
Pressure Bonding Plier, Naked Crimp Contact Naked
Cord pliers
Electrical Pliers
Wire Stripper Crimper
Crimp Pliers
Crimp Pliers
Motorcycle Crimping Pliers
Electric work pliers
Ratchet Crimp Plier